Skip to main content

Miscellaneous notes

Supported debugger probes

  • KitProg3 on-board programmer
  • MiniProg4
  • ULINK2 in CMSIS-DAP mode
  • J-Link

To use KitProg3/MiniProg4, CMSIS-DAP, and ULINK2 debuggers

  1. Select the Device tab in the Options for Target dialog and check correct core is selected:

     

  2. Select the Debug tab.
    Note:
    To use the ULINK2 probe for multi-core debugging, select the CMSIS-DAP Debugger instead of ULink for each core of the project (CM4 and CM0P).
  3. Click the Settings button.

     

  4. On the Target Driver Setup dialog on the Debug tab, select the following:
    • set Port to "SW"
    • set Max Clock to "1 MHz"
    • set Connect to "Normal"
    • set Reset:
      • For PSOC™ 6, to "VECTRESET"
      • For PSOC™ 4, PMG1, and AIROC™ CYW208xx, to "SYSRESETREQ"
      • For other devices, leave as is.
    • enable Reset after Connect option


     

  5. Select the Flash Download tab and select "Reset and Run" option after download, if needed:

     

  6. Select the Pack tab and check if the appropriate "DFP" is enabled:

To use J-Link debugger

  1. Make sure you have J-Link software version 8.12 or newer.

     

  2. Select the Debug tab in the Options for Target dialog, select J-LINK / J-TRACE Cortex as debug adapter, and click Settings:

     

  3. If you see the following message, click OK in the Device selection message box:

     

  4. Select the appropriate device in the Target device settings and click OK.

     

  5. Go to the Debug tab in Target Driver Setup dialog and select:
    • set Port to "SW"
    • set Max Clock to "1 MHz"
    • set Connect to "Normal"
    • set Reset to "Normal"
    • enable Reset after Connect option


     
  6. Select the Flash Download tab in Target Driver Setup dialog and select Reset and Run option after download if needed:

Suppress linker build warnings

Often when building an application in uVision, you will see various warnings about unused sections defined in the linker scripts, such as:
warning: L6314W: No section matches pattern EXCLUDE(*cy_smif.*).
To suppress these warnings, add "6314,6329" to the disable Warnings setting in the Options Linker tab.

Empty defines

There is a known issue in Keil µVision with empty defines. When you try to build an application, you may see an error similar to this:
error: You now need to define either
FIXED_POINT or FLOATING_POINT
To fix this, make sure empty defines are quoted. For example:
DEFINES+=FLOATING_POINT EXPORT=" " USE_CMSIS_DSP \

Patched flashloaders

Step 1: Identify the CMSIS Pack and FLM file

  • Determine the name and version of the CMSIS Pack containing the FLM file you want to overwrite (for example, AIROC_DFP.1.2.0).
  • Identify the name of the patched flashloader (the FLM file) you want to overwrite (for example, CYW208xx_SMIF.FLM). This file is located in the <app-dir>\bsps\<Kit-Name>\config\GeneratedSource directory.

Step 2: Locate the destination FLM file

  • Open File Explorer and navigate to the directory: %LocalAppData%\Arm\Packs\<Pack_Name>\<Version>\Flash
  • Replace <Pack_Name> with the name of the CMSIS Pack (for example, Infineon\AIROC_DFP) and <Version> with the version number of the CMSIS Pack (for example, 1.2.0).
  • In this directory, find the file named <FLM_File_Name>.FLM (for example, CYW208xx_SMIF.FLM).

Step 3: Overwrite the FLM file

  • Ensure that Keil µVision and any other applications using the FLM file are closed.
  • Replace the destination <FLM_File_Name>.FLM file with the patched one you want to use.
  • Make sure to keep the same file name and extension (.FLM) to avoid any issues.
Note:
When using J-Link with µVision, the flashloaders will be taken from the CMSIS DFP. So, there is no need to replace flash loaders in SEGGER J-Link software.
Last updated on