Resources tabs
For some device families, the Device Configurator contains several tabs, each of which provides access to specific resources. Different devices have different resources tabs. However, for some device families, there are no separate tabs; resources are shown in a single pane, sometimes under collapsible trees.
When you enable a resource, or select an enabled resource, the
Parameters pane
displays various configuration options. As described under
Icons
, some enabled resources may contain errors, warnings, tasks, or infos that indicate some action might be required to resolve the issue. See
Notice List
for more details.
Note:
Only the tabs relevant for a selected device are displayed, so some of the tabs may not be included for some devices.
- Tab features
Solutions tab – Options to configure multiple hardware blocks.
Peripherals – Options to enable any of the analog (if available), digital, system, and communication hardware capabilities of the chip that are not related to the platform.
Analog – For newer devices, options to enable and configure analog resources
Pins – Options for all the pin related resources.
Analog-Routing tab – For older devices, this tab shows all the analog resources, whether enabled or not, and how they connect. It also allows you to edit routes.
System tab – Options for chip-wide configuration settings such as system clocks, power management, and debug interfaces.
Memory tab – Options to allocate memory to various cores.
MMIO-Clocks tab – Options for all the MMIO clocks.
Peripheral-Clocks tab – Options for all the peripheral clocks.
DMA tab – Provides configuration of the DMA channel and transaction descriptors.