Skip to main content

GUI description

The Device Configurator GUI contains Menus, Icons, Resources tabs, and several Panes used to configure MCU peripherals.

Menus

File

  • Open – Opens an existing *.modus file. The current file, if any, will be closed.
  • Close – Closes the current file. If there are pending changes, you will be prompted to save the file.
  • Save – Saves the current file and generates code for the related application. If there are errors in the application, a dialog will indicate such. The file will still be saved.
  • Open in System Explorer – This opens your computer’s file explorer tool to the folder that contains the *.modus file.
  • Recent Files – Shows up to five recent files that you can open directly.
  • Update All Personalities – Use this item to update all resource Personalities (see Resources tabs). This opens a dialog showing all the personalities in the design.

    For example, if you load a *.modus file made with an older device support library, there might be many warnings in the Notice List to update personalities or that a personality is no longer supported. Each warning must be addressed, and doing so one at a time can be annoying. The Update All Personalities menu item addresses them all at once.

  • Exit – Closes the tool. You will be prompted to save any pending changes.

Edit

  • Undo – Undoes the last action or sequence of actions.
  • Redo – Redoes the last undone action or sequence of undone actions.

Settings

  • ModusToolbox™ Settings: This opens the Centralized Settings tool, an editor that allows you to configure a wide range of settings for your environment, such as proxy settings, content modes, and manifest DB settings. See the Settings tool user guide for more details on specific features.

View

Contains toggles to hide or show different Panes. All panes are shown by default. There is also a command to show or hide the Toolbar (hidden by default) and reset the view of the configurator to the default.

Help

  • View Help – Opens this document in either HTML or PDF format.
  • About – Opens the About box for version information, with links to open Infineon.com and the current session log file.

Device tabs

The Device Configurator can be used to configure multiple devices. All devices in the BSP display in top-level tabs above the Resources tabs.

All the settings for each Device tab are configured separately.

Note:
If you need to update or change devices, the best approach is to close the Device Configurator and then use the BSP Assistant. Refer to the BSP Assistant user guide for details.

Icons

When configuring various options with this tool, you will see the following icons:

Icon Description

Indicates there is a tooltip. Hover over the icon to display a brief message about the setting.

Enables or disables a specific resource.

There may be occasions where an error, warning, task, or info icon displays for an enabled resource. See Notice List pane for more details.

When shown in Parameters, this indicates that it is a read-only field.

When shown for a Resource, this indicates the resource is locked and disabled. There is a tooltip explaining why the resource is locked.

When shown for a Resource, this indicates the resource is locked and enabled. There is a tooltip explaining why the resource is locked.

After assigning a signal, clicking this icon jumps to the linked resource(s).

Opens a window to create, edit, and save notes.

Last updated on