Using with ModusToolbox™ application
As part of a ModusToolbox™ application, the Device Configurator
design.modus
file is an integral part of the board support package (BSP) and requires an association to an application in order to obtain device configuration information.
Installation
The Infineon Device Configurator is installed as part of the ModusToolbox™ tools package. There are no other requirements for installing this tool.
Launch the Device Configurator
You can launch the Device Configurator in various ways as described in this section; however, the tool's configuration (
design.modus
) file requires an association to an application in order to obtain device configuration information.
The
design.modus
file contains all the required hardware configuration information about the device for the application. When you save updates, the Device Configurator generates/updates source code in the
GeneratedSource
directory next to the
design.modus
file. Applications use the
design.modus
file and generated source code in future application builds.
make command
As described in the
ModusToolbox™ tools package user guide
build system chapter, you can run numerous make commands in the application directory, such as launching the Device Configurator. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:
make device-configurator
This opens the Device Configurator using the application's
design.modus
file.
VS Code and Eclipse
VS Code and Eclipse have tools to launch the Device Configurator from within an open application. Refer to the applicable user guide for more details:
Executable (GUI)
If you don't have an application or if you just want to see what the configurator looks like, you can launch the Device Configurator GUI by running its executable as appropriate for your operating system (for example, double-click it or select it using the Windows
Start
menu). By default, it is installed here:
[install_dir]/ModusToolbox/tools_[version]/device-configurator-<version>
When launched this way, the Device Configurator opens without any configuration information. You can open a specific *.
modus
file using the "Open" link or clicking
File > Open
, and then navigating to the location of the *.
modus
file to open.
Executable (CLI)
The Device Configurator executable can be run from the command line, and it also has a "cli" version of the executable as well. Running configurator executables from the command line can be useful as part of batch files or shell scripts to re-generate the source code based on the latest configuration settings. The exit code for the executable is zero if the operation is successful, or non-zero if the operation encounters an error. For more information about the command-line options, run the executable using the
-h
option.