The Project Creator tool essentially runs a "git clone" command to create one or more applications onto your computer from a remote server. It also runs the "make getlibs" command to import the necessary libraries.
Different types of applications will have different files and directory structures. After creating the application(s), navigate to the specified root directory. Inspect the files and directories located there. Use these files to modify your application(s) as necessary in your preferred environment.
Note:
The Project Creator tool generates a log file named project-creator.log in the
Application(s) Root Path. This log file captures all commands run
by the tool. It will be overwritten if you create a new application in the same
path.
Refer to the ModusToolbox™ tools package user guide for more details about make commands, BSPs, and the overall structure of ModusToolbox™ applications.