Skip to main content

Introduction

Overview

The ModusToolbox™ OpenOCD command-line interface (CLI) is based on the Open On-Chip Debugger (OpenOCD) product. OpenOCD is a powerful tool whose interface interacts with the target device via the JTAG/SWD debug ports. OpenOCD allows programming internal and external flash memories of a wide range of target devices, CFI-compatible flashes, and some CPLD/FPGA devices.

This document covers the ModusToolbox™-specific CLI extensions of OpenOCD. See the official documentation at:

http://openocd.org/documentation/

The latest released version of ModusToolbox™ OpenOCD is available from the GitHub repository:

https://github.com/Infineon/openocd/releases

Supported OS

  • Windows 11 (x64)
  • Ubuntu 22.04 "Jammy Jellyfish", Ubuntu 24.04 "Noble Numbat", Ubuntu 25.04 "Resolute Racoon"
  • macOS 14 "Sonoma", macOS 15 "Sequoia", and macOS 26 "Tahoe" (native Arm processors)

Supported devices

  • AIROC™ CYW20809 Bluetooth® LE system on chip
  • PSOC™ 6 and PSOC™ 64
  • PSOC™ 4, PSOC™ 4 HVPA, PSOC™ 4 HVMS
  • PMG1, CCGx
  • AIROC™ CYW4390x 1
  • XMC7xxx/ XMC5xxx
  • TRAVEO™ T2G Body High
  • TRAVEO™ T2G Body Entry
  • TRAVEO™ T2G Cluster 4M/6M/6M DDR MCU
  • TRAVEO™ Cluster Entry 4M MCU
  • FX3G2 and FX2G3
  • PAG2S
  • PSOC™ Control C3
  • PSOC™ Edge E84

Supported hardware (probes)

  • SEGGER J-Link stand-alone programmer (via libusbK driver for pre-2022 year probes)
  • SEGGER J-Link on-board programmer
  • Infineon KitProg3 on-board programmer
  • Infineon MiniProg4 standalone programmer
  • FTDI-based adapter on CYW954907AEVAL1F / CYW943907AEVAL1F kits

Installation

The ModusToolbox™ OpenOCD CLI software is installed as part of either ModusToolbox™ Programming tools package. Refer to the ModusToolbox™ Programming tools release notes for details.

You can also download the latest version from the GitHub repository:

https://github.com/Infineon/openocd/releases

Enable J-Link for work with OpenOCD

On Windows, to use pre-2022 year J-Link, update the driver as described in the article from SEGGER Knowledge Base of OpenOCD support. This ModusToolboxTM version of OpenOCD was tested with the libusbK v3.1.0.0 driver for the J-Link probe.

For on-board programmers and post 2022 standalone probes, configure J-Link to use native WinUSB driver as described in J-Link WinUSB driver selection.

Error codes

The OpenOCD tool returns '0' as the response code on successful completion; on a failure, it returns '1'.

1 Currently, OpenOCD does not provide a "built-in" Flash driver for the CYW4390x chip. All Flash-related operations are fully implemented in the TCL scripts. The behavior of the TCL-based driver is slightly different from the built-in one. Refer to the CYW4390x commands section for details.
Last updated on