All supported descriptors are described by USB Implementers Forum, Inc. You can find more details at

http://www.usb.org

.

The supported descriptors:

  • Device, Configuration, IAD (Interface association descriptor), Interface, Endpoint descriptors, Endpoint Companion descriptors

  • Device descriptor (Billboard), Device Qualifier descriptor

  • Audio Interface descriptor 1.0 and 2.0

  • CDC Interface descriptor

  • HID descriptor and HID Report descriptor

  • BOS descriptors:

    • USB 2.0 Extension descriptors

    • Container ID Descriptor

    • Billboard Capability Descriptor

    • Billboard Alternate Mode Capability Descriptor

    • SuperSpeed Device Capability Descriptor

    • SuperSpeedPlus Device Capability Descriptor

    • PTM Capability Descriptor

  • MS OS String descriptor

Note:

The Interface Descriptor is represented by the two items to build a tree structure: Interface Descriptor with an empty parameters pane and Alternate Settings with all Interface Descriptor parameters.

Note:

Class-Specific AS Encoder/Decoder Descriptors from USB Audio v2.0 are not supported.