About this document
A newer revision of this document may be available on the web here.
Scope and purpose
The CAPSENSE™ Tuner is used to tune CAPSENSE™ applications.
Intended audience
This document helps application developers understand how to use the CAPSENSE™ Tuner as part of creating a ModusToolbox™ application.
Document conventions
Convention | Explanation |
|---|---|
Bold | Emphasizes heading levels, column headings, menus and sub-menus |
Italics | Denotes file names and paths. |
Monospace | Denotes APIs, functions, interrupt handlers, events, data types, error handlers, file/folder names, directories, command line inputs, code snippets |
File > New | Indicates that a cascading sub-menu opens when you select a menu item |
Abbreviations and definitions
The following define the abbreviations and terms used in this document:
Application – One or more projects related to each other.
CAPSENSE – capacitive sensing
Configurator – A GUI-based tool used to configure a resource.
CSD – self-capacitance sensing method
CSX – CAPSENSE™ Transmit/Receive (CAPSENSE™ with two electrodes: Tx and Rx), mutual capacitance sensing method
ISX – inductive sensing method
IDE – integrated development environment
CSD HW – CAPSENSE™ Sigma Delta – 4
th
generation hardware (HW) block
MSC HW – multi-sensing converter – 5
th
generation hardware (HW) block
MSCLP HW – multi-sensing converter low power – 5
th
generation LP hardware (HW) block
Peripheral – Any external analog or digital device that provides an input and output for the computer.
PSOC™ – programmable system-on-chip
RTT – real-time transfer
SMARTSENSE – Auto-tuning process used for proper functionality and optimized performance of the CAPSENSE™ system.
SNR – signal-to-noise ratio
Widget – A CAPSENSE™ functional unit consisting of one sensor or a group of similar sensors, implementing a specific higher-level functionality such as Button, Proximity Sensor, Linear Slider, Radial Slider, Matrix Buttons, Touchpad, Low Power, and Liquid Level widget.
Reference documents
Refer to the following documents for more information as needed:
ModusToolbox™ tools package user guide
Eclipse IDE for ModusToolbox™ user guide
VS Code for ModusToolbox™ user guide
CAPSENSE™ Configurator user guide
Device Configurator user guide
MTB CAT1 Peripheral driver library
MTB CAT2 Peripheral driver library
Liquid-level sensing with PSOC™ 4 CAPSENSE™
Device datasheets
Device technical reference manuals