The Tuner application allows setting different configuration options with the options dialog. The settings are divided into groups.
Display options

Theme
Defines the visual style of widgets.
| Light | Dark |
|---|---|
![]() |
![]() |
SNR
See the SNR options section for a description of this tab.
Logging options

Fields:
- Log directory – Browse for the application directory where the CAPSENSE™ Tuner log files are located.
- Log file prefix – The prefix name is the user's input for the log file name. For example, <prefix_name>-<time_stamp>.csv.
- Number of samples – Defines a log session duration in samples.
- Time interval – Sets the logging interval between logged samples. Click the label to switch between milliseconds and seconds.
- Repeat header after number of samples – The header is repeated after the specified number of samples.
- Every sample on demand – Log every sample on demand.
- Data configuration check box table – Selects data to collect into a log file.
- Custom Data Settings
You can enable or disable Custom data logging. Select between Decoded active variables and Byte array. In Decoded mode, the selected variables are logged as separate CSV columns. In Byte array mode, store each byte in a separate column and in the decimal format. Custom data variables cannot be changed during active logging, so the action for changing them is disabled while logging is running. To check/uncheck all elements of the same array at the same time, press and hold the [Ctrl] key.
Advanced options

Fields:
- Device reset on connection – If this option is enabled, the target reset is performed on Connect and Disconnect for 5th generation LP CAPSENSE™ devices, which helps to establish connection even if the device was in Deep Sleep mode.
- LP command timeout (ms) – Defines the timeout for Read and Write commands for 5th generation LP CAPSENSE™ devices. During this time, the Tuner will repeatedly try to read/write data until the device wakes up from Deep Sleep and the operation succeeds. Default: 250000 ms.
- I2C response delay (ms) – Configures a delay after the ONE_SCAN command is sent and before the device response is read via the I2C communication protocol in Synchronous mode. The value indicates that the host will not make read requests until the specified time has elapsed. Recommended for long scans to prevent possible noise.