Programming and debugging are native to your chosen development environment. Infineon devices are supported in the major program and development solutions. Primarily, this means J-Link and OpenOCD. These solutions provide for programming flash within a device and provide a GDB server for debugging.
This chapter covers various topics related to building and debugging, including:
-
PSOC™ MCU programming/debugging
- Launch configurations
- PSOC™ Control: Setting the OpenOCD probe frequency
- Debug connection options
- KitProg Firmware Loader
- Supplying power with KitProg3_MiniProg4
- Power cycle programming mode with KitProg3_MiniProg4
- Switch to J-Link programmer/debugger
- Using JTAG interface in MiniProg4
- Changing programming interface SWD/JTAG
- Erasing external memory
- Programming eFuse
- Select specific CMSIS-DAP device
- Select Specific J-Link Device
- PSOC™ 4 flash security programming
- Debugging/programming for secure configuration devices
- AIROC™ Bluetooth® programming/debugging
- XMC1xxx/4xxx devices programming/debugging
PSOC™ MCU programming/debugging
Launch configurations
The flow for programming and debugging is similar for all devices. Eclipse contains several Launch Configurations that control various settings for programming the devices and launching the debugger. Depending on the kit and type of applications you are using, there are various Launch Configurations available.
There are two sets of configurations: one for KitProg3_MiniProg4 (included on-board on most Infineon PSOC™ 6 and PSOC™ 4 based kits) and another for SEGGER J-Link.


- Hello_World Program (KitProg3_MiniProg4)
- Hello_World Debug (JLink) For more information, see Debug connection options.
When an application is created, the tool generates the following launch configurations for KitProg3 by default. You can edit the Makefile to create configurations for J-Link instead. See Specify probe and generate launch configs for further details. Some items display in the Quick Panel, and some are in the Run/Debug Configurations or External Tools Configurations dialogs only.
- Attach: This launch configuration starts a debugging session attaching to a running target without programming or reset.
- Debug: This launch configuration builds the associated project, programs the project-specific output file, and then starts a debugging session.
- Erase Device: This launch configuration erases all internal memories.
- Erase All:If present, this launch configuration erases all internal and external memories.
- Program: This launch configuration builds the associated project, programs the project-specific output file, and then runs the program.
PSOC™ Control: Setting the OpenOCD probe frequency
The MTB_PROBE_FREQUENCY_KHZ variable lets
you override the OpenOCD adapter clock speed used by every debug-probe operation
(program, erase, debug). It applies to all KitProg3- / MiniProg4-based programming and
debugging flows on every supported PSOC™ Control family device, as well as the other
recipes that share the common program/IDE infrastructure.
Use it when:
- The default adapter speed is unstable on your board (long flying leads, bus extenders, level shifters).
- You need to slow the probe down for compatibility with custom hardware, or speed it up to reduce program/debug latency on a clean setup.
How to:
Define it once in the application Makefile:
MTB_PROBE_FREQUENCY_KHZ=2000
Regenerate the launch configs by clicking the option in the Quick Panel.
Debug connection options
A typical PSOC™ 6 application created for Eclipse may have launch configurations set up for one of two probes: Infineon KitProg3 (built into Infineon kits) or Segger J-Link.
| Communication Firmware | Debug Connection | More Information |
|---|---|---|
|
Infineon-provided KitProg3 |
OpenOCD via CMSIS-DAP |
https://www.infineon.com/cms/en/design-support/tools/programming-testing/psoc-programming-solutions/ |
|
SEGGER-provided J-Link DLL |
SEGGER J-Link |
KitProg Firmware Loader
The PSOC™ MCU kits include onboard programmer/debug firmware, called KitProg. The CY8CPROTO-062-4343W kit has KitProg3 by default. However, the CY8CKIT-062-BLE and CY8CKIT-062-WIFI-BT kits come with KitProg2 firmware installed, which does not work with the ModusToolbox™ software. You must update to KitProg3. KitProg3 provides the CMSIS-DAP (Bulk) protocol by default, which is up to ~2.5 times faster than the CMSIS-DAP (HID) protocol. Both modes can be used via OpenOCD.
To update it, use the ModusToolbox™ Programmer GUI or the fw-loader CLI tool. Both are provided with the ModusToolbox™ Programming tools package available from the Setup program.
For more details about these tools, refer to the ModusToolbox™ Programmer GUI user guide or the Firmware Loader user guide.
Supplying power with KitProg3_MiniProg4
If using the KitProg3 connector on a kit, power is generally supplied by the host PC. When using a MiniProg4, power is not supplied via the MiniProg4 by default. It is expected that the target MCU will be powered externally. However, the MiniProg4 does provide the ability to supply power to the target MCU.
Turning power supply on
To turn power supply on, edit the Debug/Attach Launch configurations:
- Open the Launch Configuration to modify, and select the Debugger tab.

- In the Config options field,
insert the following line (after -c "source [find
interface/kitprog3.cfg]"):
-c "set ENABLE_POWER_SUPPLY <mV>"Where<mV>defines target voltage in millivolts. For example:
- Click Apply to save the change.
And for the Program/Erase Launch configurations:
- Open the External Tools Configuration to modify in External Tools Configurations
dialog.

- In the Arguments field, add the following:
_MTB_RECIPE__OPENOCD_INTERFACE="source [find interface/kitprog3.cfg]; set ENABLE_POWER_SUPPLY <mV>;"
Where <mV>defines target voltage in millivolts. For example:

Power cycle programming mode with KitProg3_MiniProg4
By default, Launch Configurations use Reset mode to program the device. However, Reset mode is not available in all situations (for example, if the XRES pin is not available on the part's package). In these cases, Launch Configurations use an alternative reset using software. However, using the software reset type is not sufficient in some cases when access to the device's DAP is restricted (such as when set by security settings).
If there is no XRES pin available and DAP access is restricted, the only way to reset a part is to use Power Cycle mode. Follow these instructions to add commands to the launch configuration and switch to Power Cycle mode.
To update Debug Launch configurations:
- Open the Launch Configuration to modify and select the Debugger tab.

- In the Config options field, insert the following lines(after
-c "source [find interface/kitprog3.cfg]") :- For PSOC™
6:
-c "set ENABLE_POWER_SUPPLY <mV>" -c "set ENABLE_ACQUIRE 2" - For PSOC™
4:
-c "set ENABLE_POWER_SUPPLY <mV>" -c "set PSOC4_USE_ACQUIRE 2"
<mV>defines target voltage in millivolts. For example:
- For PSOC™
6:
And for Program/Erase Launch configurations:
- Open the External Tools Configuration to modify, then select the
Main tab.

- In the Arguments field add the following:
- For PSOC™ 6:
_MTB_RECIPE__OPENOCD_INTERFACE="source [find interface/kitprog3.cfg]; set ENABLE_POWER_SUPPLY <mV>; set ENABLE_ACQUIRE 2;"
- For PSOC™ 4:
_MTB_RECIPE__OPENOCD_INTERFACE="source [find interface/kitprog3.cfg]; set ENABLE_POWER_SUPPLY <mV>; set PSOC4_USE_ACQUIRE 2;"
Where <mV> defines target voltage in millivolts. For example:

Using JTAG interface in MiniProg4
The MiniProg4 can interact with the target via the SWD or JTAG protocol. By default, the SWD protocol will be used.
-c "source [find interface/kitprog3.cfg]"), insert the following lines:-c "cmsis_dap_vid_pid 0x04B4 0xF151 0x04B4 0xF152"-c "transport select jtag"

Changing programming interface SWD/JTAG
Usually MCUs support programming/debugging via SWD and JTAG interfaces. The SWD interface is the default, but you can switch to JTAG, and vice-versa.
To change target interface, update application’s bsp.mk by adding make variable as shown below (possible values are ‘swd’ and ‘jtag’) and regenerate launch configurations:
MTB_PROBE_INTERFACE=swd
Single-core projects
Kitprog3/MiniProg4
To change the target interface for KitProg3_MiniProg4, do the following:
- Open the Debug Configurations dialog and select the required configuration.
- Switch to the Debugger tab and find the "transport select ..." entry in Config options.
- Set to the value to either 'swd' or 'jtag' as applicable.

J-Link

Multi-core projects

Erasing external memory
To erase external memory use the Erase All configuration:

However, for PSOC™ 6 and PSOC™ 64 Secure Boot kits by default, erasing of external memory is turned off. To turn it on, you must modify the "Erase" launch configuration options in the External Tools Configuration as follows:
- Open the External Tools Configuration to modify, and select the
Main tab.

- In the Arguments field add the following:
MTB_ERASE_EXT_MEM=1

Programming eFuse
PSOC™ 6 MCUs contain electronic fuses (eFuses), which are one-time programmable. They store device specific information, protection settings and customer data.
By default, eFuses are not programmed even if they are present in the
programming file. To enable eFuse programming, add the following command for the Program
Configuration, under the Main tab in the Arguments field (after
-j8 program):
"_MTB_RECIPE__OPENOCD_TARGET=source [find target/$(_MTB_RECIPE__OPENOCD_DEVICE_CFG)]; psoc6 allow_efuse_program on;"
Select specific CMSIS-DAP device
If there are two or more CMSIS-DAP devices connected to your computer, the first detected device will be used by default. KitProg3 supports both CMSIS-DAP modes: HID and BULK. BULK devices are selected first, then HID devices. You can specify a CMSIS-DAP device by:
- VID and PID of the USB device
- Serial Number of the USB device
- VID, PID, and Serial Number of the USB device
There are two ways of specifying a CMSIS-DAP device:
- Add a specific command for the appropriate Debug Configuration,
under the Debugger tab in the Config options field (after
-c "source [find interface/kitprog3.cfg]"
- Modify ModusToolbox™ application's bsp.mk by adding a
MTB_PROBE_SERIALvariable, and regenerate launch configurations
Selecting by VID and PID
Use OS-specific tools to determine the VID and PID of connected devices. For example, on Windows, use the Device Manager. Use the "cmsis_dap_vid_pid" command to select a CMSIS-DAP device with a specific VID and PID. If there are two or more devices with the same specified VID/PID pair, OpenOCD uses the first detected device from the passed list.
- To specify KitProg3 in CMSIS-DAP BULK mode with VID = 0x04B4 and PID =
0xF155:
cmsis_dap_vid_pid 0x04B4 0xF155
- To specify KitProg3 in CMSIS-DAP HID mode with VID = 0x04B4 and PID =
0xF154:
cmsis_dap_vid_pid 0x04B4 0xF154
- To specify any (HID or BULK) connected KitProg3
device:
cmsis_dap_vid_pid 0x04B4 0xF154 0x04B4 0xF155
Selecting by serial number
There should not be more than one device with the same serial number. Use this method if
you want to use only one specific device. Use OS-specific tools to determine the Serial
Number of connected devices. You can also use the fw-loader utility with
--device-list option. See PSOC™ 4 flash security programming.
Use the "cmsis_dap_serial" command to select a CMSIS-DAP device with a specific Serial Number.
- To specify a CMSIS-DAP device with Serial Number = 0B0B0F9701047400 via
Debug Configuration the following command is
used:
-c "adapter serial 0B0B0F9701047400" - Alternatively, update the application's bsp.mk by adding the variable
below, and regenerate launch configurations:
MTB_PROBE_SERIAL=0B0B0F9701047400
Selecting by both VID/PID and serial number
You can use both commands together in any order directly in Debug Configuration. For example:
cmsis_dap_vid_pid 04B4 F155 cmsis_dap_serial 0B0B0F9701047400
When updating through an application's bsp.mk, add the variable below, and regenerate launch configurations:
MTB_PROBE_SERIAL=0B0B0F9701047400; cmsis_dap_vid_pid 04B4 F155;
Select Specific J-Link Device

Alternatively, update the application's bsp.mk by adding the variable below, and regenerate launch configurations:
MTB_PROBE_SERIAL=0B0B0F9701047400
PSOC™ 4 flash security programming
PSOC™ 4 devices include a flexible flash-protection system that controls access to flash memory. This feature secures proprietary code, but it can also be used to protect against inadvertent writes to the bootloader portion of flash. Refer to the device’s Architecture Technical Reference Manual for details.
Flash consists of rows (64/128/256 bytes, depending on the PSOC™ 4 device). Each row of flash can have its protection level independently set. You can assign one of two protection levels to each row, as shown in the following table:
| Protection Setting | Allowed | Not Allowed |
|---|---|---|
|
Unprotected |
External read and write, Internal read and write |
– |
|
Full Protection |
External read, Internal read |
External write, Internal write |
To apply flash security, include the appropriate data in the application by creating an array of num_rows / 8 size, where num_rows is the actual number of flash rows on the device. Each byte of this array is responsible for protection of 8 flash rows, and it sets one of two protection levels:
- 0 – unprotected
- 1 – full protection
For example, to protect the first 25 rows and the last 5 out of 256 rows, include the following array in your application:
CY_SECTION(".cyflashprotect") __USED
static const unsigned char flash_protect[0x20] =
{
0xFF, 0xFF, 0xFF, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};
To enable flash security, program the device with the updated code. If you wish to reprogram a protected device, you must first erase it.
Debugging/programming for secure configuration devices
The BootROM on devices such as PSOC™ Control and PSOC™ Edge can temporarily disable access to the core's Access Port (AP). This behavior is determined by the security policy during device provisioning. However, access can be re-enabled using a certificate (debug token). If the debugger identifies that the AP is disabled, it will upload and verify the certificate located in the "./packets/debug_token.bin" file within the current project folder.
By default, the certificate is located in ./packets/debug_token.bin in the application root folder for both OpenOCD and Segger J-Link.
OpenOCD
You can optionally make changes to the certificate’s setting using make commands and OpenOCD commands.
Make Variable (Program and Debug)
To change the location and name of the certificate (address cannot be changed)
for programming and debugging, use the make variable
CY_DBG_CERTIFICATE_PATH.
You can use the variable in the Makefile. For example:
CY_DBG_CERTIFICATE_PATH=../new_location/new_name_4_token.bin
You can also run the make variable in a terminal, and it will only apply to the specific make command. For example:
make program CY_DBG_CERTIFICATE_PATH=../new_location/new_name_4_token.bin
make erase CY_DBG_CERTIFICATE_PATH=../new_location/new_name_4_token.bin
OpenOCD commands (Debug only)
Another option to specify a different path and address for the certificate is by using the following OpenOCD commands. These apply only during a debug session:
-c "set DEBUG_CERTIFICATE %PATH_TO_TOKEN%"
-c "set DEBUG_CERTIFICATE_ADDR %HEX_ADDRESS%"

J-Link
For single-core applications, the certificate must be located in ./packets/debug_token.bin in the application root folder. Its name and location cannot be changed.
For multi-core applications, there must be multiple certificates located in ./packets/debug_token.bin in the application root folder, as well as all sub-project folders. The names and locations cannot be changed.
Multi-core debug CM33 secure application booting from RRAM

Add the following under the Startup tab under Run/Restart Commands:
For KitProg3/MiniProg4
monitor mww 0x54004054 0
monitor mww 0x54004050 4
For J-Link
monitor memU32 0x54004054=0
monitor memU32 0x54004050=4
AIROC™ Bluetooth® programming/debugging

Program configuration
This launch configuration runs a script and programs the device's memories.
- <app-name> Program: Program is used to build and program embedded applications onto the target device.
Attach configurations
The Attach configurations are used to attach to the debugger without first programming the device. They include:
- <app-name> Attach_JLink
- <app-name> Attach_KitProg3_MiniProg4
Debug settings
AIROC™ Bluetooth® devices use the JTAG SWD interface on a kit for debug via OpenOCD or J-Link probe. Typically, GPIOs need to be reprogrammed (via firmware) to enable SWD, so debug can't be performed directly after a device reset. The debugger is usually attached to a running device and symbols only are loaded.
The CYW920819EVB-02 and CYBT-213043-MESH kits have additional requirements in order to launch Eclipse debugger. In general, most debugging for these kits is done with logs and sniffers, since real time execution is usually needed for the protocols to run properly.
Refer to the AIROC™ Hardware Debugging document for more details.
XMC1xxx/4xxx devices programming/debugging
BMI for XMC1xxx/4xxx and PSOC™ Control C1xxx devices
XMC1xxx/4xxx devices use the Boot Mode Index (BMI) value to determine their boot mode and debug configuration after power-up. This value is stored in flash config sector 0.
The default boot mode is either:
- ASC_BSL (Bootstrap Loader) – for new, out-of-the-factory, devices. This mode allows erasing and programming flash via UART or SPI interface using the onboard J-Link Lite debugger and legacy Infineon tools, but does not allow programming and debugging in ModusToolbox™ and using the standalone J-Link debugger.
- SWD0 (Serial Wire Debug via Channel 0) – for Infineon kits, like XMC1100 Boot Kit. This mode allows any flash operations and debugging via the SWD interface.
There are several other modes, including using different channels (pins), SPD protocol, and flash protection scheme, which you may want to activate (switch to) during the development and production life cycles.
Refer to the following documentation for more details about BMI implementation and usage for XMC1xxx/4xxx devices.
- Boot Mode Index (BMI) XMC™ microcontrollers
- Tooling - Boot mode options XMC4000
- AN_201511_PL30_005 - Boot mode handling for XMC1000
- XMC1100 AB-Step Reference Manual
- SEGGER KBA - Infineon XMC1000: BMI - Boot Mode Index
Switching BMI with the onboard J-Link Lite debugger
With the on-board J-Link Lite debugger, you can switch the BMI using the SEGGER J-Link Commander tool, which is a part of the J-Link Software Pack that must be installed to use XMC1xxx/4xxx in ModusToolbox™.
- Connect the XMC™ Kit to USB and start J-Link Commander.
- In J-Link Commander, connect to the target device, providing its
name and specifying the SWD interface.
- Use GetBMI command to obtain the current BMI.
- Use SetBMI command without parameters to list all Boot Mode Indexes.
- Use SetBMI <index> command to set switch to desired BMI.
Switching BMI with stand-alone J-Link debugger
Stand-alone J-Link debuggers will automatically switch the BMI mode from ASC_BSL to SWD0 on target connection.
No additional steps required for programming and debugging in ModusToolbox™ if Channel 0 is used for debug pins (SWDIO - P0.14, SWCLK - P0.15).