The DFU Host tool is a cross platform utility for managing DFU firmware upgrades. The tool has both GUI and CLI interfaces.

This tool allows you to:
- Program new application data onto the supported MCU device using supported input files. See Supported devices and file formats.
- Verify the program data that is already contained on the device.
- Erase the application from the device.
- Select the *.mtbdfu file output from a ModusToolbox™ application in order to program, write, read, erase and communicate with the device.
- Abort the current operation.Note:This operation leaves the device in whatever state it is in when the abort message is acted upon.
The DFU Host tool supports communicating via I2C, SPI, UART, USB-CDC, USB-HID, and CAN-FD. They are displayed to configure their settings and view the programming status. For I2C and SPI, supported MCU should include the KitProg3 firmware module or other bridge interface, which implements USB-UART, USB-I2C, and USB-SPI bridges. For UART, communication can be done directly from the PC simply by connecting an appropriate cable. For CAN-FD, PEAK System hardware must be used.
Note:
The process of initializing the device, two CPUs
therein, and executing code in the SROM and supervisory flash, is referred to as
“bootloading”. The process of installing and updating applications in the field is
referred to as “device firmware update”. This process uses standard communication
channels (UART, I2C, USB, etc.) to download new applications
from a host.
Note:
The DFU Host tool supports Bridging mode, which allows a host
device and a companion device to be used together so that the companion device can be
programmed, verified, or erased through the connection over UART or I2C.