Skip to main content

Launch the DFU Host tool

There are several ways to launch the DFU Host tool, and those ways depend on how you use the various tools in ModusToolbox™ software.

Executable (GUI)

You can launch the DFU Host tool as a stand-alone tool without the Eclipse IDE. By default, it is installed here:

  • Windows: ~/ModusToolbox/tools_<version>/dfuh-tool/
  • Linux™: /opt/Tools/ModusToolbox/tools_<version>/dfuh-tool/bin/
  • macOS: /Applications/ModusToolbox/tools_<version>/dfuh-tool/

On Windows, you can launch the tool from the Start menu. For other operating systems, the installation directory will vary, based on how the software was installed.

Executable (CLI)

Refer to CLI description to run the dfuh-cli tool. You can also run the DFU Host tool GUI executable using the following command line arguments:

Argument Description

-?, -h, --help

Displays information on valid command-line arguments and exits..

--help-all

Displays help including Qt-specific options.

-v, --version

Displays the version information.

--debug <filename>

Appends logging information to the specified file.

Last updated on