Skip to main content

Customizing the DFU Host Tool

The DFU Host tool uses a set of timeouts for read operation before disconnecting and sending a "timeout" error. These internal configurations are suited for the development and field upgrade operations for programming the firmware or communicating with the device.

However, these configurations might require modification while debugging the DFU applications with transports using the multiple breakpoint in the target side. Due to the breakpoint, the device will pause execution and might not be able to send a response desired by the DFU Host Tool. Recommended – modify the timeout configuration and rebuild the DFU Host Tool while debugging the application using the DFU transport.

Modify the source code available in sample_code. See Example code for the appropriate path for your OS.

You can go to ~/sample_code/include/backend/cychannel.h and alter variable DEFAULT_TIMEOUT_MS. By default, it is equal to 300 milliseconds. Also, you can alter the variable DEFAULT_MAX_TRANSFER_SIZE to change the maximum allowed amount of bytes to be sent in one packet (including packet header and footer) for the GUI. By default, it is equal to 128 bytes.

After making the above modification in the source code of the DFU Host tool, build the DFU Host tool again. For details of building the DFU Host tool, refer to section Example code.

Last updated on