The DFU Host tool is provided as

GUI description

and

CLI description

.



This tool allows you to:

  • Program new application data onto the supported MCU device using supported input files. See

    Supported devices and file formats

    .

  • Verify the program data that is already contained on the device.

  • Erase the application from the device.

  • Select the

    *.mtbdfu

    file output from a ModusToolbox™ application in order to program, write, read, erase and communicate with the device.

  • Abort the current operation.


    Note: This operation leaves the device in whatever state it is in when the abort message is acted upon.

The DFU Host tool supports communicating via I

2

C, SPI, UART, USB-CDC, USB-HID, and CAN-FD. They are displayed to configure their settings and view the programming status. For I

2

C and SPI, supported MCU should include the KitProg3 firmware module or other bridge interface, which implements USB-UART, USB-I

2

C, and USB-SPI bridges. For UART, communication can be done directly from the PC simply by connecting an appropriate cable. For CAN-FD, PEAK System hardware must be used.



Note: The process of initializing the device, two CPUs therein, and executing code in the SROM and supervisory flash, is referred to as “bootloading”. The process of installing and updating applications in the field is referred to as “device firmware update”. This process uses standard communication channels (UART, I

2

C, USB, etc.) to download new applications from a host.