This section provides a simple workflow for how to use the Segment LCD Configurator.
- Launch the Segment LCD Configurator from the Device Configurator.
- On the Segment LCD Configurator toolbar, click the Edit Displays
button to open the Display Editor dialog. - On the Display Editor dialog toolbar, click the Add New
Display button. In the new row, select the Type
and specify the display Name and number of
Symbols.

- Close the dialog by clicking the X button or pressing [Esc].
- On the Segment LCD Configurator toolbar, specify the number of Common and Segment LCD connections corresponding to the mapping table dimensions. See the Mapping table section for more information.
- On the Display view, left-click and hold a pixel of the symbol, drag it
onto the mapping table below the Display view, and release the mouse button on the
desired cell.

- Repeat this process for all display pixels.
- Save the configuration and close the Segment LCD
Configurator.Back on the Device Configurator, there are several tasks in the Notice List, which correlate to the number of Common and Segment signals you configured.

- Double-click one of the task icons to jump to the Parameters pane for
the corresponding connection parameter. Click the pull-down menu and select the
appropriate signal.

- Repeat the process for every task.
- When finished, save and close the Device Configurator; see Code generation.