The Settings tool is stand-alone tool that can be launched from applicable
tools with a Settings menu, such as the Dashboard,
BSP Assistant, Library Manager, and Project Creator.


As a command-line tool
To run the Settings tool as a command-line tool, navigate to the install location and run
the mtb-settings-cli executable from a command-line prompt. By default, it
is installed here:
<install_dir>/ModusToolbox/tools_<version>/mtb-settings
For more information about command-line options, run the mtb-settings-cli
executable using the -h option.