Skip to main content

PSOC™ 6 and XMC7000/TRAVEO™ II multi-core applications

Follow steps in Create/export application for IAR Embedded Workbench. When complete, you should have a multi-core workspace similar to the following:

Then, use the instructions in this section to configure, build, program, and debug a multi-core application for PSOC™ 6 and XMC7000 multi-core applications in IAR Embedded Workbench.

Before you can launch a multi-core debug session, all projects within the workspace must be properly configured. In IAR there is a concept of 'master' and 'slave' projects. Configure the CM0+ core project as the master project, and configure the other cores (CM4 for PSOC™ 6 and CM7 for XMC7000) as slave projects.

Configure CM4/CM7 (slave) core(s)

  1. Select the CM4/CM7 core project and go to Project > Options:

     

  2. On the dialog, select the Debugger category in the Setup tab, and then select the appropriate Driver (I-jet, CMSIS-DAP, J-Link):
    ../figures/image39.png

     

  3. Enable hex file generation.
    ../figures/image45.png

    • In the Runtime Checking > Output Converter category, select the Generate additional output check box.
    • Ensure Output format is set to Intel Extended hex.
    • Click OK.

     

  4. Repeat these steps for all CM4/CM7 projects.

XMC7000/TRAVEO™ II specific steps

Some XMC7000 MCUs are triple-core devices. If you are going to use a second CM7 core in your IAR workspace, you need to implicitly set the target core in project settings so that IAR understands this project is targeting a second CM7 core. By default, IAR connects to the first CM7 core, so specifying the target core for it can be skipped.

  1. Select the project for the second CM7 core and go to Project > Options.

     

  2. Select the probe in the Debugger category, and switch to the Interface tab.

     

  3. Select the From file radio button, click Select next to the CPU label, and choose M7_1:

     

  4. Switch to the Setup tab, and select "Custom" from the Reset pull-down menu.

     

  5. In addition, specify a special linker script symbol in the project settings to distinguish CM7_0 from CM7_1, since there is a single linker script for the two CM7 cores:
    1. Select the project for the first CM7 core and go to Project > Options > Linker.
    2. Add _CORE_CM7_0_=1 in the Configuration file symbol definitions field, and click OK.


     
  6. Do the same for the second CM7 core:
    1. Select the project for the second CM7 core and go to Project > Options > Linker.
    2. Add _CORE_CM7_1_=1 in the Configuration file symbol definitions field, and click OK.
    Note:
    When debugging CM4/CM7 core stand-alone, make sure to rebuild the CM0+ project in case any changes were made, since launching a debug session only loads the CM0+ image, but does not build that CM0+ project.
  7. Build your CM7 project(s) before moving forward.

Configure and build CM0+ (master) core

  1. Select the CM0+ project and open the Options dialog.

     

  2. On the dialog, select the Debugger category in the Setup tab, and then select the applicable Driver (I-jet, CMSIS-DAP, J-Link):
    ../figures/image39.png

     

  3. Switch to the Images tab to specify the extra image to be downloaded prior to debugging in order to download images of all projects in one process.
    • Select the Download extra image check box.
    • Provide a Path to the CM4/CM7's HEX image.
    • Enter 0 for Offset.

    ../figures/image43.png

    If you provide an OUT file instead of a HEX file, the IAR IDE will fail to halt at the beginning of main() due to the main function present in both the CM0+ and CM4/CM7 OUT files.

    Note:
    For triple-core MCUs you should download two extra images.
  4. Switch to the Build Actions category.

    • Click the New button to open the Build Action dialog.
    • Paste the following command to build the CM7_0 (or CM4) project in the Command line field as single line (edit the file name for your project)
      iarbuild.exe "..\proj_cm7_0\[project-name].ewp" -make Debug
    • Select Build Order “Run before linking”.
    • Click OK to close the Build Action dialog.
    • Click the New button again.
    • Paste the following command to build the CM7_1 project (if applicable) in the Command line field as single line (edit the file name for your project)
      iarbuild.exe "..\proj_cm7_1\[project-name].ewp" -make Debug
    • Select Build Order “Run before linking”.
    • Click OK to close the Build Action dialog.

       

    The final list should look similar to this:

     

  5. Enable hex file generation. In the Runtime Checking > Output Converter category:
    • Select the Generate additional output check box.
    • Ensure Output format is set to Intel Extended hex.

    ../figures/image45.png

     

  6. Click OK, and then select File > Save All to save all the changes.

     

  7. Build the project.

Configure CMSIS-DAP/I-jet debug options

  1. Create a session configuration file.

    This is an xml file containing a projects list that should be launched in a multi-core debug session. The following shows an example for a triple-core device. For a dual-core device, remove the third partner node.

    <?xml version="1.0" encoding="utf-8"?>
    
    <sessionSetup>
        <partner>
            <name>cm0</name>
            <workspace>C:\Users\mtw-multi-core\Multicore_App\multi-core_workspace.eww</workspace>
            <project>cm0</project>
            <config>Debug</config>
            <numberOfCores>1</numberOfCores>
            <attachToRunningTarget>false</attachToRunningTarget>
        </partner>
        <partner>
            <name>cm7_0</name>
            <workspace>C:\Users\mtw-multi-core\Multicore_App\multi-core_workspace.eww</workspace>
            <project>cm7_0</project>
            <config>Debug</config>
            <numberOfCores>1</numberOfCores>
            <attachToRunningTarget>true</attachToRunningTarget>
        </partner>
        <partner>
            <name>cm7_1</name>
            <workspace>C:\Users\mtw-multi-core\Multicore_App\multi-core_workspace.eww</workspace>
            <project>cm7_1</project>
            <config>Debug</config>
            <numberOfCores>1</numberOfCores>
            <attachToRunningTarget>true</attachToRunningTarget>
        </partner>
    </sessionSetup>

     

  2. Configure multi-core debugging for the CM0+ project.
    1. Go to Project > Options -> Debugger.
    2. Switch to the Multicore tab.
    3. Select the Advanced radio button and specify a path to the session configuration file in the Session configuration field.
    4. Click OK.

    ../figures/image46.png

     

  3. Save the workspace.

Launch multi-core debug session with CMSIS-DAP/I-jet

Select the CM0 project and click the Download and debug button.

IAR builds all projects, programs all the separate images, and launches a multi-core debug session. IAR opens a separate IDE instance for each project specified in the session file. For dual-core MCUs, it should look like to this:
../figures/image47.png

The left side of the screen shows the IAR IDE instance attached to the CM0+ core. The right side shows the CM4 (or CM7) core not started yet. Once the Cy_SysEnableCM4() function is executed on the CM0+ core, the CM4/CM7 will start executing its application.

You can step through the code by switching back and forth between the two IAR IDE instances.

Launch multi-core debug session with J-Link

The IAR IDE does not have native support for the J-Link driver, which imposes some limitations:

IAR does not provide native multi-core debugging support when using a J-Link probe. This means that in order to launch multi-core debugging, you must open a few IAR IDE instances manually (one instance per core). Also, multi-core debugging with a J-Link probe lacks some features available with CMSIS-DAP and I-jet probes. Therefore, depending on the target probe, you need to configure projects slightly differently.

  • IAR will not automatically open separate IDE instances for each core, so you need to do it manually.
  • Some enhanced features are not available; see the Multi-core toolbar and CTI usage section for more details.

 

To launch multi-core debugging with J-Link:

  1. Open your multi-core IAR workspace in separate IDE instances (the number of IDE instances should be equal to the number of cores on your MCU).

     

  2. Select the CM0+ project in the first IDE instance and click Download and Debug. The debugger will download all images, reset the target, and halt at the beginning of the CM0+ project's main().

     

  3. Switch to the other IDE instances and select: Project > Attach to Running Target.
Last updated on