Overview
Manifests are XML files that tell the Project Creator and Library Manager how to discover the list of available boards, example projects, libraries and library dependencies. There are several manifest files.
- The "super-manifest" file contains a list of URLs that software uses to find the board, code example, and middleware manifest files.
- The "app-manifest" file contains a list of all code examples that should be made available to the user.
- The "board-manifest" file contains a list of the boards that should be presented to the user in the new project creation tool as well as the list of BSP packages that are presented in the Library Manager tool. There is also a separate BSP dependencies manifest that lists the dependent libraries associated with each BSP.
- The "middleware-manifest" file contains a list of the available middleware (libraries). Each middleware item can have one or more versions of that middleware available. There is also a separate middleware dependencies manifest that lists the dependent libraries associated with each middleware library.

Create your own manifest
By default, the ModusToolbox™ tools look for our manifest files maintained on our server. So, the initial lists of BSPs, code examples, and middleware available to use are limited to our manifest files. You can create your own manifest files on your servers or locally on your machine, and you can override where ModusToolbox™ tools look for manifest files.
To use your own examples, BSPs, and middleware, you need to create manifest files for your content and a super-manifest that points to your manifest files. To see examples of the syntax of super-manifest and manifest files, you can look at files provided on GitHub:
- Super-manifest: https://github.com/Infineon/mtb-super-manifest
- Code example manifest: https://github.com/Infineon/mtb-ce-manifest
- BSP manifest (including dependencies): https://github.com/Infineon/mtb-bsp-manifest
- Middleware manifest (including dependencies): https://github.com/Infineon/mtb-mw-manifest
Make sure you look at the "fv2" manifest files if you are using the flow for ModusToolbox™ version 2.2 and later.
The manifest system is flexible, and there are multiple paths you can follow to customize the manifests.
- You can create supplementary super-manifest files that identify additional content. The tools will merge your additional content with the default super-manifest.
- You can replace the default super-manifest file used by the tools.
Supplementing super-manifest using manifest.loc
In addition to the standard super-manifest file, you can specify "custom" super-manifest files. This allows you to add additional items (BSPs, code examples, libraries) along with the standard items. You can do this by creating a manifest.loc file in a hidden subdirectory in your home directory named ".modustoolbox":
<user_home>/.modustoolbox/manifest.loc
For example, a manifest.loc file may have:
# This points to the IOT Expert template set
https://github.com/iotexpert/mtb2-iotexpert-manifests/raw/master/iotexpert-super-manifest.xml
If this file exists, then each line in the file is treated as the URL to another super-manifest file, which is exactly like the standard super-manifest file. The data from these manifests is combined with data from the standard super-manifest. See the Conflicting data section for dealing with conflicts.
Replacing standard super-manifest using variable
The location of the standard super-manifest file is hard coded into all of the tools.
However, you may override this location by setting the
CyRemoteManifestOverride environment variable. When this variable is set,
the tools use the value of this variable as the location of the super-manifest file and the
hard-coded location is ignored. This removes all Infineon content from the tools, by
default. For example:
CyRemoteManifestOverride=https://myURL.com/mylocation/super-manifest.xml
Processing
The process for using the manifest files is the same for all tools that use the data:
- The first level is to access the super-manifest file(s) to obtain a list of manifest files.
- The second level is to retrieve the manifest data from any packs that were installed.
- The third level is to retrieve the manifest data from manifest.loc file, if it exists.
Conflicting data
Ultimately, data from all of the super-manifest and manifest files are combined into a single data collection of BSPs, code examples, and middleware. During the collation of this data, there may be conflicting data entries. There are two types of conflicts.
The first kind is a conflict between data that comes from the level 1 primary super-manifest (and linked manifests), data that comes from the level 2 pack manifest, if present, and data that comes from the level 3 manifest.loc file, if present. In this case, the data in the level 2 pack manifest overrides the data from the level 1 standard super-manifest, and the data in the level 3 manifest.loc file overrides the data in the level 2 pack manifest. This mechanism allows you to intentionally override data that is in the standard location. In this case, no error or warning is issued. It is a valid use case.
The second kind of conflict is between data coming from the same source (that is, both from primary or both from secondary). In this case, an error message is printed and all pieces of conflicting data are removed from the data model. This is done because in this case, it is not clear which data item is the correct one.
Local content storage
The Local content storage (LCS) feature provides a command-line tool called lcs-manager-cli that allows you to create your own local, offline content on demand.
For more details, refer to the LCS Manager CLI user guide.