Skip to main content

Create new memory file

  1. Select New *.cymem File… to open the Edit Memory window from the main QSPI Configurator:
    ../figures/image10.png

  2. Click [ . . . ] button next to the Location field to specify the file name and location of the memory configuration file (*.cymem). If you prefer, you can ignore the Location field for now, and then specify the file name and location when saving the file.
  3. Enter a desired Memory Part Number. When selected, this field will be displayed in the main QSPI Configurator window in the Memory Part Number.
  4. Complete the information for the remaining fields, as appropriate. See Edit memory file fields.
  5. Click Save to save the configured memory. If Location was not specified previously, this will open a save dialog to navigate to the appropriate location, type a file name, and click Save.
  6. Click Close to return to the QSPI Configurator.

Memory database

The QSPI Configurator memory database is a set of default memory configurations, based on values from each memory’s datasheet. Check that the selected memory configuration is aligned with a particular part number.

Note:
By default, some memory parts are configured with protected regions, which prevents the successful execution of program/erase memory commands.
Note:
Dummy cycles may vary based on memory part configuration.
Note:
The list of supported commands may vary between memory parts.
Last updated on