Skip to main content

AIROC™ CYW20829 application

Follow steps in Create/export application for IAR Embedded Workbench.

Fix vector table

There is a known issue with an invalid for IAR name for the vector table in the C start-up code. To resolve it:

  1. Open the Options dialog and select the Debugger item under Category.
  2. Select the Extra Options tab, select the Use command line options check box, and paste the following command-line option:
    --drv_vector_table_base=__Vectors


     

  3. Click OK to close the Options dialog.

Build, program, debug

To build, save the application and select Project > Make. The Output should display the progress, ending with text similar to this:

Total number of errors: 0
Total number of warnings: 0
Resolving dependencies...
Build succeeded

To program, select Project > Download > Download file… and select the [project_name].final.hex file in [project_root]\build\last_config [you might have to switch to All Files (*.*)].

 

To debug, select Project > Debug without Downloading.

Last updated on