Skip to main content

GUI description

The EZ-PD™ Configurator GUI contains menus, the main toolbar, and tabs with toolbars to configure the various parameters, as well as Notice List and Status bar to provide indications

Menus

File

  • New – Creates a new file with new configuration.
  • Open – Opens the configuration file.
  • Close – Closes the configuration file.
  • Save – Saves the existing file.
  • Save As – Saves the existing file under a different name.
  • Open in System Explorer – Opens your computer’s File Explorer browser to the directory that contains the *.mtbezpd file.
  • Exit – Closes the configurator.

Edit

  • Add Port – Adds a new Port tab to configure parameters.
  • Remove Port – Removes the selected Port tab.
  • Copy Port – Copies port settings of the selected port to the clipboard.
  • Paste Port – Pastes port settings from the clipboard to the selected port; replaces current settings.
  • Undo – Undoes the previous change.
  • Redo – Redoes the last undone change.

View

  • Notice List – Shows/hides Notice List. The pane displays by default.
  • Toolbar – Shows/hides the toolbar.
  • Reset View – Resets the view to the default.

Help

  • View Help – Opens this document.
  • About EZ-PD™ Configurator – Opens the About box for version information, with links to open https://www.infineon.com and the current session log file.

Notice List

The Notice List pane combines notices (errors, warnings, tasks, and infos) from many places in the configuration into a centralized list. You can double-click a notice location to show the parameter causing the error or warning. For more information about the Notice List, refer to Device Configurator user guide.

Status bar

The status bar displays various information, including a file operation status, hints, input field ranges, etc. On the right side, it displays the selected device.

Toolbar

The toolbar contains common commands from the File and Edit menus, such as New, Open, and Save. Use the check box under the View menu to show or hide the toolbar.



Port tabs

This area contains one or two tabs to configure various parameters. Each tab includes a toolbar with the following commands:



  • Add/Remove PDO – Adds or removes a PDO from the selected list.
  • Sort PDOs – Toggles Sort on and off. When enabled, this reorders the PDOs by type and voltage.
  • Move Up/Down – When Sort is disabled, these move the selected PDO up or down in the list.
  • Expand/Collapse All – Expands or collapses the entire tree of items in the Port tab.

Parameters and values

The following sections describe the parameters available for each category. Select a parameter category to see that category individual parameters and values as appropriate on the right pane of the EZ-PD™ Configurator.

Port Information



The Port Information node consists of the following parameters:

Field name Description Valid range

Manufacturer Vendor ID (0x)

Vendor ID assigned to manufacturer by USB-IF

0x0000 – 0xFFFF

Manufacturer Product ID (0x)

16-bit Product ID that identifies the product

0x0000 – 0xFFFF

Manufacturer Name

Manufacturer name string

Maximum 21 ASCII Characters

Port Role

Power handling role of the device

0 -> Sink

1 ->Source

2 -> Dual Role

Default Port Role

Default power handling role of the device

0 -> Sink

1 -> Source

Current Level (mA)

Operating current range for the device

0 -> 900 mA

1 -> 1.5 A

2 -> 3 A

Cable Discover Count

Number of cable discovery attempts to be made

0x00 – 0x14

DRP Toggle Enable

Whether Rp-Rd toggle is enabled in unattached state

Check box enabled or not.

Rp Supported (mA)

Rp values supported by the device

Bit Mask

Bit 0 -> 900 mA Rp

Bit 1 -> 1.5 A Rp

Bit 2 -> 3 A Rp

PD Operation Enable

Whether USB-PD operation is supported on the port

0 -> No

1 -> Yes

Preferred Power Role

Whether Try.Src or Try.Sink is enabled for the port

0 -> No Try.Src or Try.Sink supported

1 -> Try.Src supported

2 -> Try.Sink supported

Port Disable

Whether the PD port is to be disabled at start-up

Check box enabled or not.

Cable Discovery Enable

Whether cable discovery is enabled as part of the source state machine

Check box enabled or not.

Dead Battery Support

Whether dead battery operation is supported

Check box enabled or not.

Error Recovery Enable

Whether Type-C error recovery is enabled for this port

Check box enabled or not.

FRS Config

Fast Role Swap feature enabled flags

0 -> None

1 -> FRS receive enable

2 -> FRS transmit enable

VCONN Retain

Whether Vconn supply should be left enabled even if the EMCA's cable VDO indicates that Vconn is not required.

Check box enabled or not.

Accessory Mode Enable

Whether accessory mode is to be enabled

Check box enabled or not.

Rp Detach Enable

Option to enable/disable disconnect detect mechanism using Rp in Sink role

Check box enabled or not.

Port Type

Port type in Source_Info data object. Indicates whether the amount of power the port can provide is fixed or can change dynamically

0 -> Shared Capacity Port

1 -> Assured Capacity Port

Port Maximum PDP

The maximum amount of power the port is designed to deliver

0x00 – 0xFF

Port Present PDP

The amount of power the port is presently capable of offering

0x00 – 0xFF

Port Reported PDP

The amount of power the port offering in its Source_Capabilities or EPR_Source_Capabilities message.

0x00 – 0xFF

PD Revision Major

PD revision major

0x0 – 0xF

PD Revision Minor

PD revision minor

0x0 – 0xF

PD Version Major

PD version major

0x0 – 0xF

PD Version Minor

PD version minor

0x0 – 0xF

PDO

This node represents the set of Power Data Objects (PDOs) for the selected device. The PDOs supported by the device are arranged hierarchically. PDOs can be Source PDOs or Sink PDOs, depending on whether they describe the power sourcing or sinking capabilities of the USB-PD device. All fields listed under the Source PDOs and Sink PDOs nodes are defined in the USB-PD specification, revision 3 classified as follows:

  • Fixed Supply
  • Battery
  • Variable Supply
  • Programmable Power Supply
  • Adjustable Voltage Supply

You can add or remove PDOs using Add/Remove PDO buttons available in Port tabs. Each PDO contains an Enable check box, which specifies whether the PDO is enabled at system start-up.

Source PDOs

The Source PDOs node displays only when the value of Port Role parameter is set to Source or Dual Role in Port Information node.

The parent Source PDOs node contains the following parameters from 5V Fixed Supply Source PDO.



 

Fixed Supply Source PDO configuration parameters



 

 

 

Battery Source PDO configuration parameters



 

Variable Supply Source PDO configuration parameters



 

Programmable Power Supply Source PDO configuration parameters



 

Adjustable Voltage Supply Source PDO configuration parameters



 

Sink PDOs

The Sink PDOs node displays only when the value of the Port Role parameter is set to Sink or Dual Role in the Port Information node. Sink PDO configuration includes two additional parameters:

  • The Sink Give Back parameter specifies whether the feature is enabled for this PDO.
  • The Min/Max Operating Current parameter specifies the minimum current required for device operation if give back is enabled. If give back is disabled, this field specifies the maximum operating current that may be required.

 

 

 

 

The parent Sink PDOs node contains the following parameters from 5V Fixed Supply Sink PDO.



 

Fixed Supply Sink PDO configuration parameters



 

Battery Sink PDO configuration parameters



 

Variable Supply Sink PDO configuration parameters



 

Programmable Power Supply Sink PDO configuration parameters



 

EPR Configuration

This contains a check box to enable or disable Extended Power Range (EPR) configuration.



EPR Source PDOs

Enable EPR Source to display one or more EPR Source PDOs.

Fixed Supply



Adjustable Voltage Supply



EPR Sink PDOs

Enable EPR Sink to display one or more EPR Sink PDOs.



 

 

 

 

 

The EPR Sink PDOs configuration parameters:

Fixed Supply



 

Adjustable Voltage Supply



SCEDB Configuration

This pane contains a check box to enable or disable the SCEDB parameters based on the USB-PD specification, revision 3, section 6.5.1.





SKEDB Configuration

This contains a check box to enable or disable the SKEDB parameters based on the USB-PD specification, revision 3, Section 6.5.13.



Last updated on