There are numerous ways to launch the EZ-PD™ Configurator, and those ways depend on how you use the various tools in ModusToolbox™.

make command

As described in the

ModusToolbox™ tools package user guide

build system chapter, you can run numerous make commands in the application directory, such as launching the EZ-PD™ Configurator. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:

make ez-pd-configurator

This command opens the EZ-PD™ Configurator GUI for the specific application in which you are working.


Executable (GUI)

If you don't have an application or if you just want to see what the configurator looks like, you can launch the EZ-PD™ Configurator GUI by running its executable as appropriate for your operating system (for example, double-click it or select it using the Windows Start menu). By default, it is installed here:

<install_dir>/ModusToolbox/tools_<version>/ez-pd-configurator-<version>

When launched this way, the EZ-PD™ Configurator opens without any settings configured. You can either open a specific configuration file or create a new one. See

Menus

for more information.


Executable (CLI)

The EZ-PD™ Configurator executable can be run from the command line, and it also has a "cli" version of the executable as well. Running configurator executables from the command line can be useful as part of batch files or shell scripts to re-generate the source code based on the latest configuration settings. The exit code for the executable is zero if the operation is successful, or non-zero if the operation encounters an error. For more information about the command-line options, run the executable using the

-h

option.