The Settings tool includes the following options for configuration:
Operating Mode (3.x version only)
This setting provides access to the Local Content Storage (LCS) feature, which provides a command-line tool called lcs-manager-cli to create your own local content on demand. You can decide whether to save the entire database (approximately 5 GB of data) or a subset of data for the BSPs that you specify. Refer to the ModusToolbox™ Local Content Storage CLI user guide for more details.

Proxy Server

Manifest DB (3.x version only)
The manifest database determines the available BSPs and libraries used for your applications. In some cases, you may not be able to access the default location of the database. This is often an issue for users in corporate environments that block access to some sites.

Select the desired option with the value editor:
- Default Manifest DB - Standard Infineon URL on GitHub
- Default China Manifest DB - Standard URL for China users
- Advanced Settings: - Custom URL with the following options:
- User defined manifest DB URL: Specifies a specific location of the manifest database for ModusToolbox™ tools, for example https://mycompany/mtb-super-manifest/v2.X/mtb-supermanifest-fv2.xml.
- Git insteadOf - old value: This provides a value, for example GitHub.com/Infineon, that Git will use to switch to a new value.
- Git insteadOf - new value: This provides a new value, for example mycompany.com/mtbmanifest, that Git will substitute for the old value.
Refer to the ModusToolbox™ tools package user guide for more details about manifests.
Information Level

- Low: Displays spinner when downloading Git repos.
- Medium: Displays numerical representation of progress, as well as any running sub-commands.
- High: Includes spinner, running sub-commands, and visual representation of progress.
Enabled EAP (3.x version only)
If you have an early access pack (EAP) installed, this setting allows you to choose the enabled EAP from the list or disable the EAP. When you select an EAP from the list, it will automatically get enabled when you click Save.

Global content path (3.x version only)

Local Content Storage Location (3.x version only)

manifest.loc file path (3.x version only)

Default SDK
The default SDK setting allows you to select a virtual SDK in various tools like Project Creator and Library Manager. A virtual SDK is a list of assets (kits, applications, libraries, etc.) and specific versions of those assets. For more information on using virtual SDKs, refer to the Project Creator user guide.

Git safe.directory configuration (3.x version only)
This setting creates a temporary Git configuration used to avoid errors caused when cloning Git repositories from shared local folders. Use the value editor to turn the feature on and automatically create a temporary configuration. Alternatively, you can use the value editor to turn the feature off and configure Git manually.

Check EAP on app load (3.x version only)
This setting enables a check when an early access pack (EAP) is active to ensure that the application contains libraries from that EAP. While this setting is meant to improve the overall user experience with EAPs, you can choose to disable the check feature for your project, if needed.

Custom Git executable
If the default version of Git bundled with the tools package does not work properly, this setting allows you to specify a different Git installation by entering the path to its executable.

Tools Paths