The active BSP for the application displays in bold text with "(ACTIVE)"
next to it. An application can only have one active BSP. If your application has more than
one BSP included, select one of the other BSPs to be active by clicking the radio option
next to it. You can also choose to right-click on it and select Set as Active BSP. Then, click the Update button.


When you click the Update button, the system displays progress in
the message console and updates your application's Makefile
TARGET= variable to specify the new BSP as active.