Skip to main content

PSOC™ 64 secure single-core application

Follow instructions in Create/export application for Keil µVision. The project creation process also generates an ide_postbuild.bat file used to execute postbuild commands for the application. When complete, use these instructions to configure, build, and debug your application.

Note:
For a PSOC™ 64 secure MCU, you must also follow the instructions in the Secure Boot SDK user guide to generate keys and provision the device.
  1. Select Project > Options for Target 'Target 1'… to open the Options dialog.
  2. Select the User tab and enable the Run #1 check box under After Build/Rebuild. Then, enter ide_postbuild.bat \"#L\".

     

  3. Select the Utilities tab and select the project.ini file using the […] button.

     

  4. Then, click OK to close the options dialog.
  5. Select Project > Build Target to build the application and execute post-build commands.

After performing these steps, you should be able to run debug, erase, and program for PSOC™ 64 secure MCUs.

Last updated on