Skip to main content

Revision history

Revision Date Description of Change

**

2018-10-26

New kit guide.

*A

2018-11-08

Updated Introduction.

Updated Description.

Updated KitProg3 Tools Support and Compatibility.

Updated Installing and Using KitProg3.

Updated Using KitProg3.

Updated Programming and Debugging.

Updated description.

Updated Mode Switching.

Updated description.

Updated KitProg3 Design.

Updated KitProg3 LEDs.

Updated description.

Updated KitProg3 vs. KitProg2.

Updated description.

Updated Troubleshooting.

Updated description.

*B

2018-11-22

Added PSOC™ Creator/PSOC™ Programmer information

*C

2019-02-19

Updates throughout for KitProg3 v1.1 and DAPLink

Updated Introduction.

Added DAPLink Mode.

Updated KitProg3 User Interface.

Updated Troubleshooting.

Updated KitProg3 Operating Speeds.

Updated KitProg3 Status LEDs.

Updated Downgrading to KitProg2.

Updated Upgrading to KitProg3.

*D

2019-02-21

Remove listing of an unsupported kit

*E

2019-05-29

Updated DAPLink CMSIS-DAP HID protocol to DAPLink CMSIS-DAP Bulk protocol

Updated description of Mode Switching between HID, Bulk and DAPLink interfaces

Added description of Mode Switching between CMSIS-DAP Bulk with two UARTs and UART + bridging

Added new supported kits for KitProg3 firmware

Added DAPLink CMSIS-DAP v2 driver issue on Windows 7 into Troubleshooting section

*F

2019-07-24

Minor edits.

*G

2019-09-26

Added new supported kits for KitProg3 firmware

Updated description of status LEDs behavior

Added section 6 Updating KitProg3

Updated Update DAPLink Firmware and Upgrading to KitProg3 sections.

Removed Downgrading to KitProg2 section.

*H

2019-12-12

Updated mode switching diagram

Added description about UARTx2 mode

Updated KitProg3 Status LEDs.

Added new supported kits for KitProg3 firmware

Updated figure of KitProg3 High-Level Architecture

*I

2020-03-18

Updated KitProg3 High-Level Architecture figure

Updated mode switching diagram

Updated mode switching information for CMSIS-DAP HID

Added new supported kit for KitProg3 firmware in DAPLink mode

Updated KitProg3 vs. KitProg2 section

Updated lists of supported IDEs for KitProg3 firmware in sections Introduction, DAPLink mode and Installing and Using KitProg3

Added information about JTAG programming via MiniProg4

Added information about MiniProg4 in DAPLink mode

Updated Operating speeds table in KitProg Design section

Added DAPLink driver issue on Windows 10 into Troubleshooting section

*J

2020-06-11

Clarified LED connection in section 2.2.1.

Updated list of supported kits in section 3.1 and section 4.1.

Clarified Troubleshooting process for updating drivers in Chapter 7.

*K

2020-07-28

Updated KitProg3 Tools Support and Compatibility.

Added Windows driver issues into Troubleshooting section

Added information about using simultaneous use of the USB-I2C/SPI bridging and debugging in Windows

*L

2020-08-19

Added footnotes about Serial Port limitation on macOS in section 3.2 and section 4.3.2

*M

2021-01-29

Updated Launching a Debug Session in Eclipse IDE for ModusToolbox™ picture in section 2.2.2.

Updated mode switching information in section 2.2.3.

Added Bridging Features section 2.2.5.

Updated list of supported kits in section 3.1.

Updated list of supported baud rates in section 3.2.

Updated footnote about Serial Port limitation on macOS in section 3.2.

Updated DAPLink Serial Port information in section 4.3.2

Updated Updating KitProg3 information section 6.

Updated solution to DAPLink CMSIS-DAP v2 issue on Windows 7 in section 7.

*N

2021-04-20

Added reference to KitProg Host Protocol Interface in section 2.2.5

Added note on Supported kits in section 3.1

Added example of "device-name" in section 6.1.3

Updated Operating speeds table in section 3.2

*O

2021-08-12

Updated list of supported devices in section 3.1

Updated list of supported baud rates in section 3.2

Updated footnote about Serial Port limitation using custom communicational library on macOS in section 3.2.

Added footnote about intervals between UART frames in section 3.2

Updated mode switching from DAPlink to Uartx2 mode in section 2.2.3.1

Added information about switching to Uartx2 mode via firmware loader tool in section 6.1.3

*P

2022-05-02

Added note for DAPLink mode availability in the next release in section 1

Updated sections 3.1 and 2.2.5.2 with information about usage of GPIO Bridging feature

Added section 6.1.3 Documentation on fw-loader tool

Removing references to Mbed OS, including KitProg3 High-Level Architecture in Figure 1-1.

Updated list of supported devices in section 3.1.

*Q

2023-04-13

Updated Troubleshooting section with possible COM port issues and ways to solve them

Added info on UART flow configuration in section 2.2.5.1

Updated Kit Support table with availability of the UART HW Flow Control feature support in section 3.1

Removed info regarding deprecated support of Mbed CLI from Troubleshooting section

*R

2024-04-26

Removed info regarding no longer supported Windows 7 from Troubleshooting section

Updated section 2.2.5.1       USB-UART Bridge Feature

Updated and reformatted list of supported devices in section 3.1

Updated links/references to and screenshots of ModusToolbox™ Programmer throughout document

*S

2024-10-28

Updated list of supported kits in section 3.1 and section 4.1.

*T

2025-02-21

Fixed font size in Kit-Support 3.1 table in section 3.1

Updated list of supported kits in section 3.1 and section 4.1

Fixed command typos in section 2.2.5.2

*U

2025-04-22

Updated list of supported kits in section 3.1

Updated Fig. 2.1 and 5.1

Last updated on