| Library | Details | Docs |
|---|---|---|
| wifi -mw-core | The Wi-Fi Middleware Core library bundles the core libraries that any Wi-Fi application needs. This has been deprecated. | API reference |
| wifi-host-driver | The Wi-Fi Host Driver (WHD) is an independent, embedded driver that provides a set of APIs to interact with our WLAN chips. | API reference |
| wifi-connection-manager | The Wi-Fi Connection Manager (WCM) provides easy to use APIs to establish and monitor Wi-Fi connections on our devices that support Wi-Fi connectivity. | API reference |
| wifi-core- freertos-lwip-mbedtls | This repo comprises core components needed for Wi-Fi connectivity support. The library bundles FreeRTOS, lwIP TCP/IP stack, mbed TLS for security, Wi-Fi host driver (WHD), wifi connection manager (WCM), secure sockets, connectivity utilities and configuration files. | API reference |
| wifi-resources | This repo contains clm and nvram files for the supported Wi-Fi boards from associated chip set. | API reference |
| whd-bsp-integration | This library provides some convenience functions for connecting the Wi-Fi Host Driver (WHD) library to a BSP that includes a WLAN chip. | API reference |
| smartcoex | Provides an API to configure the coex parameters for WLAN and Bluetooth® Low Energy on platforms with Wi-Fi & Bluetooth® combo chip. | API reference |
| enterprise-security | This library implements a collection of the most commonly used Extensible Authentication Protocols (EAP) used in enterprise Wi-Fi networks. | API reference |
| wpa3-external-supplicant | The WPA3 External Supplicant supports WPA3 SAE authentication using HnP (Hunting and Pecking Method) using RFC https://datatracker.ietf.org/doc/html/rfc7664 and H2E ( Hash to Element Method) using RFC https://datatracker.ietf.org/doc/html/draft-irtf-cfrg-hash-to-curve-10 and following 802.11 spec 2016. | See links to the left. |
| ethernet-connection-manager | Ethernet Connection Manager (ECM) is a library which helps application developers to manage ethernet connectivity for XMC7200 devices. | API Reference |
| ethernet-core-freertos-lwip-mbedtls | This repo comprises core components needed for ethernet connectivity support for XMC7200 devices | API reference |
| ethernet-phy-driver | Provides the Ethernet PHY-related interface APIs as required by Ethernet connection manager library to enable the completion of Ethernet-based applications on supported platforms. | API reference |
| lwip-network-interface-integration | This library is an integration layer that links the lwIP network stack with the underlying Wi-Fi host driver (WHD) and Ethernet driver. This library interacts with FreeRTOS, lwIP TCP/IP stack, Wi-Fi host driver (WHD), and Ethernet driver. It contains the associated code to bind these components together. | API Reference |
| nonrtos-lwip-mbedtls | Contains core components needed for non-rtos connectivity support. The library bundles lwIP TCP/IP stack, mbed TLS for security, connectivity utilities and configuration files. | API reference |
| rtlabs-uphy-lib | Partner library for with support of RT-Labs Industrial Communication stack on XMC7000. | RT-Labs u-phy website |
ModusToolbox™ for Wi-Fi and ethernet
Last updated on