All ModusToolbox™ applications require a target BSP. Infineon provides BSPs
for all of our kits, as well as generic BSPs for each chip architecture, to use as a
starting point. When working with your own hardware, you can modify an Infineon BSP to
match that hardware, or you can create a BSP by specifying the device(s) it contains. The
BSP Assistant helps to simplify the process of creating or modifying a BSP to suit your
needs.


Note:
WICED_BTSDK BSPs and ModusToolbox™ version
2.x BSPs are not supported by the BSP Assistant at all. In addition, the following features
are not supported in the BSP Assistant:
- Modular BSPs
- Multi-MCU BSPs (The MCU explicitly named in the bsp.mk file is supported, but the other MCU is not changeable using the BSP Assistant.)