Plots created in Waveform Viewer can be annotated with labels to indicate features of interest or to otherwise convey information to human readers.
Note that you can see and work with labels only if their display is switched on, which is
indicated by the activated state of the Show/Hide Labels toolbar button:
. If the
button is not activated (
), click it to show labels before you work with them. (This
does not affect axis labels, which are always visible.)
Note, too, that standard and point labels can only be added to the selected plot. Select the desired plot before using either of these tools.
Standard labels
Standard labels are similar to Post-it notes that you can pin on a plot. They are anchored to a spot on the plot where you click the tool and are scrolled with the plot. If the plot is zoomed, they remain the same size. If the plot is deleted, the label is also deleted.
To add a label to the selected plot, make sure
that labels are displayed (see above) and click the
toolbar button. This opens the Label dialog in which you can
enter the text that you want to display. You can also specify the font and
background color of the label, as well as its orientation and the alignment of the
text within the label. When you click OK in the dialog, the
mouse pointer indicates you note text, and clicking in the selected plot positions
the label there.
To reposition an existing label, drag it around with the mouse.
To edit the text or style of a note, double-click it. This opens the Label dialog in which you can make changes as desired.
To delete a label, select it and click
in the
toolbar.
Point labels
Point labels are very similar to standard labels, and most of the information given above also applies to them. The main difference is that point labels include a line which is anchored to a point of the plot. They also add a box around the label text.
Therefore you click twice when creating a point label: The first click positions the anchor point where the line starts, and the second click positions the box with the text.
When repositioning point labels, dragging the text repositions it but leaves the anchor point where it is, and dragging the point leaves the text where it is. Dragging the connecting line repositions all elements together.
Annotating axes
While labels cannot be attached to axes with the label tools, you can add titles or other descriptive text in the axis settings.
To do so, select the axis that you want to label and choose or click
in the toolbar. (For details on selecting
an axis, see Working with axes .) In the Axis Settings dialog that opens, check the Custom option in the X Axis
Label or Y Axis Label section,
respectively, and enter the text in the text field. If you want to show the custom
text in place of (as opposed to in addition to) the standard axis label, uncheck the
Standard option.