Skip to main content

Model Libraries view

The Model Libraries view presents all available standard components that have been made available by Infineon and other sources and that you can use in your circuits.

Each device typically would contain a set of its own symbols. These symbols, components and other schematic data are contained in a library. When you simulate your environment with the use of a specific device, then download a library and the various elements in the library can be arranged according to your application for the simulation. This saves looking for the items required in the vast ocean of elements because you can find the required subset in the library.

Download Manager

for information on using the Download manager, see Managing Infineon and third-party components.

Download the required library by means of the Download Manager by clicking the icon .

Filter the list to ease your search by either
  • Component
  • Container
  • Category
  • Tag

A window pops up and this can then be sorted for Components, Circuits, Automotive only. Select the required library and download.

Basic Components
You have a choice of various standard circuit components to drag and drop onto your schematic. Basic components are listed in the Model library as well as on the task bar in the work area as follows:
Capacitor
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position.
Controlled sources
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position. You can choose from a number of controlled sources as listed below:
  • Voltage-controlled current source (vccs)
  • Voltage-controlled voltage source (vcvs)
  • Current-controlled current source (cccs)
  • Current-controlled voltage source (ccvs)
Current Source
Drag and drop onto work area, press the Esc key. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position. You can choose from a number of current sources as listed below:
DC
Variable/Behavioral
Pulsed
Sinusoidal
PWL
Current-controlled current source (cccs)
Voltage-controlled current source (vccs)
Diodes
You have a number of diodes from which to choose depicted in the menu.
  • Ideal Diode
  • Zener Diode
  • Schottky Diode
  • Model based Diode
Ground
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position.
VDD Jumper
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position.
Ideal Transformer
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position.
Inductance
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position.
NC
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position.
Resistor
Drag and drop onto work area, press the Esc key to complete. You can also right-click to trigger the Place command. Move your mouse onto the work area and place your component in the desired position.
Infineon Components

Download Infineon components from the Download Manager. Downloaded components appear in the categories as listed below.

These circuits are prebuilt. You need to save it with a different name because all Infineon components are read-only.

Two categories of Infineon components in the components list are:

Circuit Testbench depending what you downloaded from the Download Manager, can include Power Management and Automotive

Power depending what you downloaded from the Download Manager, can include gate-driver-ics, mosfet and igbt

Last updated on