Skip to main content

Creating a schematic

Schematics are created in the Workspace view and populated in the work area.

Before you begin

The tutorial project must have been created, as described in Creating a project. It must contain an empty schematic.

About this task

In this example, you will create a simple low-pass filter.

Procedure

  1. If the empty schematic is not already open, open it by double-clicking its file in the Workspace view.


    The schematic is displayed in the work area.



  2. Place the voltage source.

    We are using a sinusoidal voltage source, which is a basic component.

    The following steps show how to place such components from the model libraries, which works in the same way for more complicated components. Basic components can also be placed using the toolbar icons in a schematic view. Except for how the desired component is chosen, the procedure is the same as described here.

    1. In the Model Libraries view, open the Basic Components section by clicking the triangle in front of its name, and then open Voltage Source.
    2. Drag the entry Sinusoidal from the library to the work area.


      Instead of dragging the component, you can also double-click it in the library.

      The cursor changes its form to indicate that you can now place sinusoidal voltage sources.

    3. Click the mouse in the location where you want to put the voltage source.
    4. Press Esc to return to the standard cursor.

      If you do not press Esc or choose a different component, you can continue clicking to place additional voltage sources.

    The schematic now contains a sinusoidal voltage source.

  3. Zoom in to get a better view of the component.

    To do so, click the Zoom In tool until the voltage source symbol is large enough or click the Zoom Region tool and drag a conveniently sized rectangle around the area on which you want to zoom in.

    You should now be able to clearly see the symbol in the schematic.



    The dots in the background indicate the grid that can assist you in correctly placing and aligning components.

  4. Edit the properties of the voltage source to fit the schematics’ requirements.
    1. Choose the Select Mode tool and double-click the voltage source.

      Alternatively, you can also select the voltage source and press Q or right-click it and choose Properties.

      The Properties dialog opens.



      The dialog lists all available parameters of the selected component. Parameters that are mandatory are highlighted in yellow. Brief explanations of the parameters are available by hovering the mouse over the parameter name.

    2. Enter the following values: VO 0, VA 1, FREQ 1MEG, TD 0. Click OK.
      The most important of the specified values are displayed beside the voltage source.


  5. In the same manner as the voltage source, drag a capacitor, a ground, and a resistor to the schematic.

    Do not modify these components’ parameters.

  6. Select the resistor, right-click it, and choose Rotate from the context menu.

    Your schematic now looks similar to this:



  7. Connect the components with wires.
    1. Choose the wire tool .
    2. Click the upper pin of the voltage source and then click the left pin of the resistor.
      Both pins are connected by a wire-
    3. In the same way, connect the resistor to the capacitor and the ground to the capacitor and the voltage source.

    The schematic now looks like this:



  8. Label the wires to the resistor.
    1. Choose the wire labeling tool .

      The Wire Name dialog opens:



    2. Enter IN as the wire name and click OK.
    3. Click the connection between the resistor and the voltage source.
      The wire is labeled “IN”.
    4. Choose again, enter OUT as the wire name, and click the wire from the resistor to the capacitor.
      The wire is labeled “OUT”.

    The wires are now labeled:



    These labels can be referenced when setting up the simulation.

  9. Press Ctrl+S to save the schematic.

Results

You have created a schematic for a simple low-pass filter the operation of which can be simulated in InfineonSpice.

What to do next

Set up. the simulation as described in Setting up a simulation.

Last updated on