Skip to main content

Creating a new project

New projects are created by clicking the New Project button.

About this task

A new project is typically created to model a new device.

Procedure

  1. Click the button at the top of the Workspace widget.
    You can also press Alt+N or choose File > New > New Project.
    The New Project dialog opens.
  2. Enter a name for the new project and click OK.

    The name may contain letters (a-z), numbers (0-9) and some special characters, such as: # & () + - = @ [] ^ ' {} ~. A dot (.) can also be used except at the end; an underscore (_) can be used except at the beginning of the name. For more information, see Naming directories and files.



Results

The project appears in your workspace.

The project already contains an empty schematic with the same name as the project.



What to do next

Creating a new schematic
Last updated on