Simulations are set up by specifying the desired parameters for them in the Simulation Environment view.
About this task
Setting up a simulation includes specifying the desired result categories, simulation parameters, and output options. While it is possible to run a simulation with default settings, getting the information required in a particular stage of the development usually requires an appropriate setup for the simulation.
Specifying a setup includes entering numerous values. Options for doing so are described in Values and expressions.
and
(standard and differential, respectively). You can
also define expressions to plot based on signals by double-clicking the