Click File and a list of options related to managing files, such as to open, save, print and import data and exit, appears.

- Open
- Click or select
to open a saved fíle in your selected location.
- Open with Layout
- Open with Layout means that not only do you get the waveform but also get all of the toolbars including all of the icons, and Output Variables
- Reset
- Click Reset or
to change your
layout back to the default view. If you zoomed into the graph or
rearranged the windows, all of these actions will be reversed to the
default.
- Save
- Secure all changes by clicking Save or
.
- Save As
- Saves the output of this simulation with a name of your choice.
- Export CSV
-
Click Export CSV.
A window, Export variables to CSV opens. appears and you give the file a name or browse to overwrite an existing file.

Click Add and a Select Variable(s) window open. Here you choose from the available list of variables that are included in these plots. Remove allows the removal of your variables in case you change your mind.
Within the Select Variable(s) window, Output Variables contains a search field where you type the variable you require and the rest of the list empties out if it does not match your search. Remaining in the list is the item for which you have searched. On the bottom right of the Select Variable(s) window, you can select variables according to their position in case you have several plots open.
Click OK to proceed with your selection. Click Cancel to abort Select Variable(s).

If you clicked OK you will have the variables for export in the Variables window.
The Limit x-range option lets you restrict the export to a specific range. The Exponential view Precision defines how many decimal places after the decimal point anywhere between 0 and 15. You can set the Delimiter which is what will separate the various data units.
Once you have completed all the settings, click Export. A window opens indicating the folder in which you can find your file:C:\Users\user-name\AppData\Local\Programs\Infineon\InfineonSpice\InfineonSpice-version\bin
Alternatively, click Cancel to abort the process.
- Print Preview
- You can view what you would obtain if you printed the waveform before printing.
- Click Print and a window opens where you may choose how many copies you wish. You can also choose to Collate, specifically arrange printed documents in a specific order, assembling each set of pages in the correct sequence or Print First Page First or Print Last Page First. Click Print and an explorer window opens where you then select the location of the printout in PDF format.
- Print Setup
- Set all desired settings for the Printer, Orientation, Copies, Colour mode, Print to file → Slide button Off or On and Pages → All pages or Custom range.
- Export as SVG
- Export the diagram as a standard vector graphic (SVG) instead of PDF which is the output of the Print menu.
- Copy to Clipboard
- If you would like to paste the waveform to another any other, for example, Microsoft Office application, click on Copy to Clipboard
- Close No Save
- Click on Close No Save and you close the Waveform Viewer window. Nothing is saved.
- Close
- Select Close and a window opens where you can choose to save changes but only if you made any edits. You can also check the box for whatever selection you choose as your default.