Skip to main content

System Requirements

The following system requirements have to be fulfilled in order to use the InfineonSpice Software.

  • Windows 10
  • Minimum of 4 GB RAM
  • Approximately 815MB of disk space
  • Network connection for installation, licensing and content access

InfineonSpice does need a license to run - a default license is shipped with the installation. You need to be connected to the internet during the installation process and the first time you use the software in order to validate your license. After that it will be validated periodically.

Note:
The software is not supported on 32-bit operating systems.
Last updated on