Skip to main content

Custom Installation

This chapter explains the custom installation of InfineonSpice on your computer.

Run the InfineonSpice_2026.2_Windows_x64.exe installer and follow the prompts.

First of all you can select the install mode. Choose if you want to install the software only for you (recommended) or for all users.

Figure 1. Select install mode


Read the license agreement document presented on the next page of the installation wizard and select I accept the agreement. The installation cannot proceed without this. Click Next to proceed. Or click Cancel if you wish to close the installation wizard.

Figure 2. License Agreement


On the next page please choose Custom Installation and proceed with Next.

Figure 3. Custom installation


If you wish to read the Release Notes you can follow the link in the Information field.
Figure 4. Information


Press Next and choose the location for the installation on your local disk. By default, the InfineonSpice Software will be installed to:

C:\Users\<User>\AppData\Local\Programs\Infineon\InfineonSpice\2026.2

Figure 5. Destination Location


Note:
If you change the default path it might be necessary to install the software as administrator in order to run properly
Note:
You can change the directory, but do not use spaces in the installation directory name. Also, do not use common illegal characters, such as: / : * ? " < > |. Refer to Naming directories and files

Keep or enter a destination for the installation and press Next to proceed.

You can choose a Start Menu folder where to place the program's shortcut.

Figure 6. Start Menu Folder


Click Next to proceed or Back to return.

The InfineonSpice installer can create a desktop shortcut for you and it is enabled by default. Click Next to proceed.

Figure 7. Create Desktop shortcut


The next page shows a summary of actions to be performed by the installer. Please verify the items before proceeding. Click Install.

Figure 8. Ready to install


The following wizard will display the progress of the installation.
Figure 9. Installing


After the installation process has been completed you can choose to directly run InfineonSpice and display the Release Notes. If you do not want it, just un-tick the according option and click Finish.

Figure 10. Installation complete


Whenever you wish to cancel the installation process in between press Cancel and choose Yes in the following prompt.
Figure 11. Cancel installation


Last updated on