Skip to main content

Attributes dialog

The Attributes dialog lets you view and modify properties of elements in a symbol.

The dialog is opened by selecting the desired element in a symbol view and choosing Edit > Properties. The command is not available when multiple elements are selected.

Depending on the type of the selected component, different versions of the dialog are shown:

Clicking the OK button applies the settings in the dialog to the selected element and closes the dialog. Clicking Cancel closes the dialog without making changes to the element.

Pin Attributes tab

The Pin Attributes tab lets you modify the properties of a pin.



Name

The name of the pin.

Visible

Whether the pin name is visible in the symbol.

Direction

The direction of the pin: input output, or both.

Type

Whether the pin is represented in the symbol by a square or a circle.

Property Name

(Currently under review.)

Default Net Name

The default name for the wires that are connected to the pin.

This information is optional.

Sensitive

(Currently under review.)

Pen Attributes tab

The Pen Attributes tab lets you modify the stroke properties of a closed shape, a line, or an arrow.



Style

Whether the shape has an uninterrupted (solid) stroke or the stroke is composed of dots, dashes, or a combination of the two.

Width

The width of the stroke.

Brush Attributes tab

The Brush Attributes tab lets you modify the fill properties of a closed shape or an arrow.



Brush Style

Whether the selected shape is just an outline (hollow) or filled (solid).

Arrow Attributes tab

The Arrow Attributes tab lets you modify the dimensions of an arrow tip.



Length

The length of the tip of the arrow. Higher numbers create longer tips.

Width

The width of the tip of the arrow. Higher numbers create tips with wider bases.

Last updated on