A menu is a set of options presented to the user of a computer application to help them find information or execute a function. Menus are common in GUIs. Depending on what kind of content is displayed in the frontmost tab, different commands are available in the menu.
Open InfineonSpice and the following menus appear on the menu bar:
Additional menus can become visible if the frontmost tab is an editing tab of the appropriate type: