TriCore™ AURIX™ 2nd Generation Family

About this document​

Scope and purpose​

This document introduces the ReqIF XML format, the digital and machine-readable format that will be provided together with PDF versions of the user manual and errata sheet. An explanation of how PDF-based document content is mapped into the ReqIF format is provided, including relevant tools that can be used to further analyze or process Infineon digital documentation.

Intended audience​

The intended audience for this document is software engineers, requirement engineers, application engineers, developers of electronic systems, and other technicians using the microcontroller documentation in automatized ways or aiming to integrate it into their own environment.

ReqIF XML format high level overview​

ReqIF is an XML-based Requirement Interchange Format that provides a common interface of requirements. With its roots in the automotive industry, the ReqIF format provides lossless requirement exchange and workflow integration.

As a meta model, this format provides an XML schema that is used as a common data model across supporting tool environments. Workflows of different companies can be interconnected by this format; this format provides status information about deliverables in a way that the receiving company can use dependent linking on certain features.

The inventors: Object Management Group (OMG)​

The ReqIF format was originally introduced by the OMG to provide a method of requirement interchange between different companies, having limited access to the original requirement databases.

For the current used version of the format

( ReqIF 1.2)

, OMG shares the specification, normative and informative documents on their webpage.

Example scenario​

Company A provides a certain functionality that is used as a fundamental part in the development of Company B’s product. An early exchange of information in the ReqIF format can provide preliminary objects that can be used to further refine the development process in Company B.

Especially in the automotive industry, where the development is often tied to norms like the functional safety standard ISO 26262, this early available exchange can provide a basic structure for development of customer parts in advance and provide objects that can be used in the V-development model proposed by ISO 26262.

ReqIF files provided with the PDF version of a user manual or an errata sheet uses the structure defined by the ReqIF format and wrap chapters into these requirement containers. As a result, these documents are machine-readable. This enables customers to use them either directly as linkable objects for further development or to use algorithms for analyzing and automating the (pre-)processing for content analysis.

Providing requirement containers of the documentation on a chapter level enables more granular tracking of the documents content. To leverage integration into machine processing and requirement engineering, certain elements within the content is marked with additional meta-data. Main purpose of these metadata is, to easily identify and track certain elements and make them visible by conversion tooling. This supports actual information about what a certain element like a bitfield means, without the need of heuristic approaches to identify them. By doing so, robustness of both: the file format and further processing is increased. Focus for this metadata marking are registers. Elements within a register container are tagged based on the IP-XACT standard. This standard is provided by the SPIRIT consortium and has the goal to make IP description and configuration compatible across different vendors.

Proposed tools to use ReqIF​

For ReqIF files, the main tool designed for reading and manipulating the content is the

ReqIF Studio

from ReqIF Academy. It provides a common overview of the requirements provided by the ReqIF format and allows a structured view of provided requirements. In addition, requirement engineering tools can be directly used to integrate the objects from ReqIF into a requirement environment.

For automating in a more generic way, XML-focused processing engines like XSLT or XML parsers allow extracting the information or its subset for further processing. An outlook on potential applications is given at the end of this document.

ReqIF Studio​

Infineon will use the ReqIF XML format as a container to wrap our document information. ReqIF Studio will show one requirement entry per chapter or register of the underlying document.

Figure 1. AURIX™ TC39x errata sheet opened as ReqIF in ReqIF Studio


Beside a complete machine-readable version of the document, every chapter is split into its own container (highlighted in green), providing a document-unique identifier and version (highlighted in orange). This allows easy tracing of changes within the document itself and enables to create linkable objects in requirement databases that support the ReqIF format.

In addition, the full structure that reflects the document’s table of contents (ToC) is listed (highlighted in blue) for easy navigation. Because registers are the focus to become accessible for processing as requirements, every register is put into its own wrapping container. This results in one unique requirement object per register.

Requirement engineering tools​

To provide a requirement-based work environment, many tools are compatible with the ReqIF format. Seamless integration of external provided requirements in these tools provide easy access of traceability measures based on exchanged requirements.

As the choice of the right requirement engineering tooling highly depends on individual environments, multiple tools are available. A short overview of some of the most used tools, supporting the ReqIF standard is provided in the following list:

Information classifier based on the IP-XACT standard​

Because the ReqIF format does not have the IP-XACT standard built in, but only provides certain structures to hold the metadata, the documents content is structured in XHTML using attribute-based classification of the content. This enables using more specific classifiers that are connected to the very minimum content it describes.

The document’s register content is wrapped in metadata, which is based on the 2018

IP-XACT standard

. Because the main point of view for the IP-XACT standard is on the bitfield level while our documentation is focused on the register level, additional identifiers that are not part of the original IP-XACT standard maybe required. These identifiers will be added as part of the customized extensions and allow to map the content between bitfield-based and register-based views.

Metadata which is used in our ReqIF XML files are shown in

Mapping of document content into ReqIF format

.

Example use case​

As shown in

Figure 2

, the granularity of the requirement provided in ReqIF is at the register level. This helps to easily make registers linkable as objects in requirement databases; however, this lacks details if requirements need to be linked to bitfields, for example. This is important especially when registers share layouts or are addressable via different bus addresses. In such cases, it is hard to differentiate between them when dealing only at the register level.

Figure 2. Default granularity by having one requirement container per register


If ReqIF provides metadata only on the requirement level, a classification applies to the whole paragraph of the requirement. For a register description that refers to multiple bitfields, the granularity is not fine enough to allow the classification of each referred bitfield individually; instead, it only provides a summary of these elements inside the requirement.

For better machine readability and processing capability, this metadata is moved into the XHTML domain of the ReqIF format, allowing to map the additional information directly to these elements. Because this view is used for machine processing, it allows better integration for automated analysis when working at the file level. In general, providing a capability to further process files in an automatic way improves usability and integrateability when compared to manual integration of large documents.

Figure 3. ReqIF shown on XML level in Oxygen XML Editor providing more details


As

Figure 3

shows, making use of the wrapping structures inside the ReqIF format allows to add more granular metadata. When comparing the XML view to the ReqIF Studio view, multiple registers that share the same layout are much more than the same requirement now. It can easily be distinguished between different registers, even when sharing the same layout and shown as the same register view in the user manual. The metadata at the XML level allows to distinguish between these registers (highlighted in green). In addition, coherent content is delimited by the XML structure and provides disjunct blocks of content for further processing. As an example, the offset address of each corresponding register is structured at the same level (highlighted in blue) as the corresponding register name (green), but within one wrapping parent element.

IP-XACT classifier used​

The following IP-XACT classifiers are used in the ReqIF format for the user manual and errata sheet:

Table 1. Used IP-XACT classifier

IP-XACT metadatum

Used for

Structure

Ipxact_longName

Full name

Register

Ipxact_description

Description text

Register

Ipxact_name

Short name

Register

Ipxact_addressOffset

Offset address

Register

Ipxact_field

Bitfield definition

Bitfield

Ipxact_name

Name

Bitfield

Ipxact_description

Description text

Bitfield

Ipxact_access

Access type

Bitfield

Ipxact_bitoffset_bitwidth

Bitfield offset and range

Bitfield

Ipxact_enumeratedValue

Enumeration of bitfield values

Bitfield

Because the standard is focused on bitfield view, there are some classifiers which slightly deviate from the original. As an example,

ipxact_bitoffset_bitwidth

is actually a combination of two identifiers:

ipxact_bitoffset

and

ipxact_bitwidth

. In Infineon documentation, bits and bitfields are specified as the offset inside the register and when spanning multiple bits, as an array [x:y]: there is no separate value for the actual size. Instead, the size can be derived as the difference between starting and ending bits.

Mapping of document content into ReqIF format​

This section provides a better insight on how the actual information is stored in the ReqIF format in comparison with the user manual or the errata sheet, a mapping overview is provided, highlighting which information of the PDF document will be mapped to which part of the ReqIF format. This enables to use the ReqIF format provided to interpret or further process the information for integration into a customer-specific environment.

For easier navigation, the structure of an example erratum and an example register from the user manual is shown here, providing a split into sections.

Figure 4. Sections in an erratum


Figure 5. Sections of a register description


For easier accessibility, each element of the document is described first with its meaning and then further mapped into the IP-XACT standard, showing how these are represented in the ReqIF format. These sections are used to support the orientation inside the PDF structure, which should be known already.

The following mapped elements that are available in the documents are described with their abstract meaning and how these are mapped into the ReqIF format using XHTML structures and metadata as XML attributes.

Figure 6. User manual register-header section mapped into ReqIF


Figure 7. User manual bitfield definition section mapped into ReqIF


Figure 8. Errata sheet headline mapping into ReqIF


Figure 9. Errata sheet description mapping into ReqIF


Outlook: Using ReqIF for automation​

This section gives an overview of benefits when using digital documentation in the ReqIF format using most obvious applications. Additional use cases are possible.

Integration for requirement-driven development​

As the documentation is provided as requirements in the ReqIF format, it can be imported into requirement tools. This provides linkable targets for requirement development based on Infineon microcontrollers. Main benefits here are finer granularity when it comes to traceability and less manual work.

Instead of creating linkable objects in a requirement environment out of the PDF version of the documentation, the documentation can simply be imported. This reduces the effort and time in going through the PDF document and manually migrating the content into the databases and is also less error prone due to little manual impact.

How to identify if a document update is affecting implemented applications​

When making use of identifiable elements like registers, signals, or bitfields, tooling can be implemented to process a new delivery of a document. By identifying these structures, which are used by an implementation in user code or as part of the requirement engineering, it can easily be compared with a tool-based generated delta of deliveries. This helps to identify and highlight affected updates in an application. A significant benefit here is that the documents can be parsed by a program and basic information of affecting changes for different structures can be provided.

An example is when an application uses signal X and a register Y. Tool-based processing of the ReqIF delivery can easily identify if either X (signal) or Y (register) are affected without having to manually go through the whole document. As the documents can be imported into a requirement environment, this allows traceability of an application change due to documentation with already provided requirements.

Early feedback and alignment between customers and deliverables​

By providing documentation in a machine-readable format, integration at the customer side can be improved, reducing possibility of errors introduced by manual work and allows easier traceability between different devices and versions.

Having this in an early stage of development, open points and mismatches between application requirements and device implementation can be identified. This enables early feedback and deeper development integration.

Revision history​

Document revision

Date

Description of changes

V01_00

2023-12-07

Initial version

V1.1

2025-05-27

Template update.

Updated the terms ReqIF, DOORS, Polarion and Jama Connect to align with the latest branding guidelines.