Attention:

Be aware that after applying Kill mode your device will be permanently locked from any external debugger or programmer software. This operation is not reversible.

  1. Connect the device to the host computer and select it in the

    Programmer

    ,

    Board

    , and

    Device

    drop-downs.

  2. To use Kill mode, go to

    Options > Programmer Options

    and enable it in

    PSOC 4 Kill Mode

    drop-down.



  3. Connect to the device (see Connect Device).

  4. Click the

    Chip Protection

    pull-down and select

    Kill

    mode.

    A warning message asking for confirmation is displays.



  5. Click

    Yes

    to apply Kill mode for your PSOC 4, PMG1, PAG2S and CCGx.

When the operation completes, the log is appended with a message, and the device is disconnected from the programmer automatically.