1. Connect the device to the host computer and select it in the

    Programmer

    ,

    Board

    , and

    Device

    drop-downs.

  2. Select the programming file as described in the

    Load programming file

    section.

  3. Connect to the device (see

    Connect device

    ).

  4. Select the

    Reset Chip

    check box under

    Program Settings

    .

  5. Click the

    Program

    button.

ModusToolbox™ Programmer programs the device and displays various messages in the Log. Then, a message in the Status Bar indicates that the device was programmed successfully or that an error occurred.



The target device is reset and running.