1. Connect the device to the host computer and select it in the

    Programmer

    ,

    Board

    , and

    Device

    drop-downs.

  2. Select the programming file as described in the

    Load programming file

    section. The programming file should contain valid eFuse data region (at address 0x90700000).

  3. Select the

    Program Security Data

    check box under

    Program Settings

    .



  4. Connect to the device (see

    Connect device

    ).

  5. Click the

    Program

    button.

ModusToolbox™ Programmer programs the device and displays various messages in the Log. Then, a message in the Status Bar indicates that the device was programmed successfully or that an error occurred.



If some eFuse bits have been already programmed before, a warning message "The efuse bit at address xx has been already blown" appears in

Log

.