You can program the flash of an AIROC™ CYW20829 device in Secure lifecycle mode only by providing a valid debug certificate file.

  1. Connect the device to the host computer and select it in the

    Programmer

    ,

    Board

    , and

    Device

    drop-downs.

  2. Select the programming file as described in the

    Load programming file

    section.

  3. Click on the

    Debug Certificate

    option under

    Program Settings

    and select the certificate file in the dialog.

    The path will display under Settings.


    Connect to the device (see Connect Device).

  4. Connect to the device (see

    Connect device

    ).

  5. Click the

    Program

    button.