Verify device with External Memory
Connect the device that supports external memory (for example, CY8CKIT-062-WiFi-BT with QSPI support) to the host computer and select it in the
Programmer
,
Board
, and
Device
drop-downs.
Select the programming file as described in the
Load programming file
section. The programming file should have external memory region(s).
Select the
External Memory
option under
Program Settings
.

Connect to the device (see
Connect device
).
Click the
Verify
button.
ModusToolbox™ Programmer verifies the device and displays various messages in the
Log
. Then, a message in the Status Bar indicates that the device was verified successfully or that an error occurred.