Program binary file with Offset
Connect the device to the host computer and select it in the
Programmer
,
Board
, and
Device
drop-downs.
Select the binary programming file as described in the
Load programming file
section.
Connect to the device (see
Connect device
).
Enter the desired address in the
Offset
field under
Program Settings
.
Click the
Program
button.
ModusToolbox™ Programmer programs the device and displays various messages in the Log. Then, a message in the Status Bar indicates that the device was programmed successfully or that an error occurred.

Note:
Offset options is available only for binary programming files.