1. Connect the device to the host computer and select it in the

    Programmer

    ,

    Board

    , and

    Device

    drop-downs.

  2. Select the programming file as described in the

    Load programming file

    section.

  3. Connect to the device (see

    Connect device

    ).

  4. Click the

    Verify

    button.

ModusToolbox™ Programmer performs the Verify device operation and displays various messages in the Log. Then, a message in the Status Bar indicates that the device was verified successfully or that an error occurred.