1. Connect the device to the host computer and perform recover device procedure as described in

    How to recover AIROC™ Bluetooth® devices on failure

    .

  2. Click the Programmer pull-down and select 'WICED Bluetooth-PortXX' programmer.



    Note:

    The CYW9M2BASE-43012BT board should be switched to Dual UART mode first, otherwise the WICED Bluetooth programmer will be unavailable in theBoardpull-down menu. To do this, press the hardware 'Mode' button on the Kit, hold it for 3 seconds, then release it.

  3. Open the

    Board

    pull-down and select the appropriate board name (e.g., CYW955513EVK-01)

  4. Select the programming file as described in the

    Load programming file

    section.

  5. Connect to the device (see

    Connect device

    ).

  6. Click the

    Program

    button.

ModusToolbox™ Programmer programs the device and displays various messages in the Log. Then, a message in the Status Bar indicates that the device was programmed successfully or that an error occurred.