Verify custom flash regions
Connect the device to the host computer and select it in the
Programmer
,
Board
, and
Device
drop-downs.
Select the programming file as described in the
Load programming file
section.
Connect to the device (see
Connect device
).
Expand Verify Regions option in Program Settings to see the list of flash regions available for verification. By default, only supported by target device regions are displayed:
application
AUXflash
Sflash
eFuse
QSPI

Right-click on
Verify Regions
or any region entry to open the context menu.

To add a custom flash region, select
Add Region
. Select the added list entry, and enter the correct values for start and end addresses of the region.

To remove any region in the list, right-click the desired region entry and select
Remove Region
.

To revert any previous change, select
Undo
.
When finished with the list of regions, start device verification by clicking the
Verify
button on the toolbar.

You can also select
Verify
on the context menu.

ModusToolbox™ Programmer verifies only the regions specified in the
Verify Regions
list. Then, a message in the Status Bar indicates that the device was verified successfully or that an error occurred.
To reset the
Verify Regions
list to its default state select
Reload Regions
from the context menu. This action will remove all custom regions and load default regions corresponding to the flash map.