This feature is supported by AIROC™ CYW20829 devices, as well as PSOC™ Edge E84, XMC7100/7200 and CYT4Bx MCUs. It allows you to specify the patched flashloader file in FLM format along with the appropriate QSPI configuration. Patched flashloaders contain data about how your external memory is configured.

  1. Connect the device to the host computer and select it in the

    Programmer

    ,

    Board

    , and

    Device

    drop-downs.

  2. Select the programming file as described in the

    Load programming file

    section.

  3. Select the

    External Memory

    option under

    Program Settings

    (if supported).

  4. Click on the

    Flashloader

    option under

    Program Settings

    and select the patched flashloader (FLM) file in the dialog.

    The path will display under

    Settings

    .



  5. Connect to the device (see

    Connect device

    ).

  6. Click the

    Program

    button.

Note:

To be able to program custom QSPI memory, you should also provide the appropriate QSPI configuration file (qspi_config.cfg) generated by the ModusToolbox™ QSPI Configurator tool. This file should be placed in the same directory as the patched flashloader file; it is located and read by ModusToolbox™ Programmer automatically.

Refer to the QSPI Configurator User Guide for more information about patching flashloaders.