1. Attach and select a device that supports external memory (for example, CY8CKIT-062-WiFi-BT with QSPI support).

  2. Select the

    External Memory

    option under

    Program Settings

    .



  3. Select the programming file as described in the

    Load programming file

    section. The programming file should contain external memory region(s) and correct QSPI configuration data.

  4. Select

    Erase/Program USER/TOC/KEY allowed

    option under

    Probe Settings > Sflash Restrictions

    . This is only needed for PSOC™ 6 devices.

  5. Connect to the device (see

    Connect device

    ).

  6. Click the

    Program

    button.

ModusToolbox™ Programmer programs the device and displays various messages in the

Log

. Then, a message in the Status Bar indicates that the device was programmed successfully or that an error occurred.